About LDO for SNVS

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
1,137件の閲覧回数
Edgard
Contributor III

Dear an Engineer,

 

I'm wondering what LDO I should choose. 

On the RT1020 EVMK circuits, there is UM1750S-00. 
But UM1750S-00 is minor LDO, it is a little bit difficult to purchase in my country.

I have a question, dose "SNVS loard regulation" require the ability of max 350mA current?
I found other LDO and it was max 300mA current.

Thanks in advance.

ラベル(1)
0 件の賞賛
返信
1 解決策
1,113件の閲覧回数
kerryzhou
NXP TechSupport
NXP TechSupport

Hi @Edgard ,

   Thank you for your interest in the NXP MIMXRT product, I would like to provide service for you.

   In fact, the MIMXRT1020-EVK is using the DCDC in default, although the LDO is added, but not used, you can see, the resistor to the LDO is DNP:

kerryzhou_0-1692599127320.png

So, if you use the DCDC like the EVK, LDO don't need to use:

kerryzhou_1-1692599150375.png

If you need to use the LDO for the SNVS,  300mA current is also too much larger, as you know, our SNVS is uA current, you also can select more smaller LDO.

kerryzhou_2-1692599233715.png

 

Wish it helps you!

Best Regards,

Kerry

 

 

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
1,114件の閲覧回数
kerryzhou
NXP TechSupport
NXP TechSupport

Hi @Edgard ,

   Thank you for your interest in the NXP MIMXRT product, I would like to provide service for you.

   In fact, the MIMXRT1020-EVK is using the DCDC in default, although the LDO is added, but not used, you can see, the resistor to the LDO is DNP:

kerryzhou_0-1692599127320.png

So, if you use the DCDC like the EVK, LDO don't need to use:

kerryzhou_1-1692599150375.png

If you need to use the LDO for the SNVS,  300mA current is also too much larger, as you know, our SNVS is uA current, you also can select more smaller LDO.

kerryzhou_2-1692599233715.png

 

Wish it helps you!

Best Regards,

Kerry

 

 

0 件の賞賛
返信
1,108件の閲覧回数
Edgard
Contributor III
Dear Kerry

thanks for your advice.
I could understand. I'll try to design the circuits without LDO.

Kindest Regards
Edgard