Hi.
how to build u-boot.imx and kernel image through yocto for mfgtools, we use BSP 4.4.3_r1 uboot version 2014.04 kernel 3.10.53
below as my step.
mkdir fsl-yocto
cd fsl-yocto
repo init -u git://git.freescale.com/imx/fsl-arm-yocto-bsp.git -b imx-3.10.53-1.1.0_ga
repo sync
MACHINE=imx6qsabresd source fsl-setup-release.sh -b ./build-x11-mx6qsabresd -e x11
echo "UBOOT_CONFIG = \"emmc\"" >> conf/local.conf //we use EMMC boot .
MACHINE=imx6sxsabresd bitbake -c deploy u-boot-imx
to here.
i can see the <UBOOT> directory build-x11-mx6qsabresd/tmp/work/imx6sxsabresd-poky-linux-gnueabi/uboot-imx/2014.04-r0/git
question A how to build this image?
below ifno Description in the office document file.
#!/bin/bash
export ARCH=arm
export CROSS_COMPILE=<path to cross compiler prefix> (e.g.
/opt/poky/1.4.1/sysroots/i686-pokysdk-linux/usr/bin/cortexa9hf-vfp-neon-poky-linux-
gnueabi/arm-poky-linux-gnueabi-
make distclean;
make mx6<custom board name>_config
make
where is the directory for "/opt/poky/1.4.1/sysroots/i686-pokysdk-linux/usr/bin/cortexa9hf-vfp-neon-poky-linux-"?
can i user the android directory prebuilts/gcc/linux-x86/arm/arm-eabi-4.6/bin/arm-eabi- to compile this image?
question B how to build kernel image for mfgtools?
there office document show as below
bitbake fsl-image-mfgtool-initramfs
where is the kernel code source? I need at what directory to exec that command?
and i saw the command
bitbake fsl-image-gui
when exec it .where is the code direcotry? how to compile it?
can i get what from this command. bitbake fsl-image-gui bitbake core-image-base
can i get what from this command.bitbake fsl-image-mfgtool-initramfs?
what info is my need? I Just only want to build uboot and kernel image for mfgtools.
why the document "Freescale_Yocto_Project_User's_Guide.pdf" is hard to read?
thanks verymuch!
解決済! 解決策の投稿を見る。
I think this is useful for you
The Yocto Project™ and Linux® Software Development for i.MX Application Processors
On page 72 for the details of MFGtool
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
http://www.freescale.com/infocenter/index.jsp?topic=%2FQORIQSDK%2F3135308.html
and
http://www.freescale.com/infocenter/index.jsp?topic=%2FQORIQSDK%2F3138992.html
Have a great day,
Pavel
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi pav.
thanks for your reply.
I had get some code by below command.
mkdir ~/yocto
cd ~/yotco
repo init -u git://git.freescale.com/imx/fsl-arm-yocto-bsp.git -b imx-3.10.53-1.1.0_ga
repo sync
MACHINE=imx6qsabresd source fsl-setup-release.sh -b ./build-x11-mx6qsabresd -e x11
echo "UBOOT_CONFIG = \"emmc\"" >> conf/local.conf
MACHINE=imx6sxsabresd bitbake -c deploy u-boot-imx //get uboot source
cd ~/yocto
MACHINE=imx6qsabresd source fsl-setup-release.sh -b build-x11 -e x11
bitbake fsl-image-gui
bitbake fsl-image-mfgtool-initramfs //there i found the direcotry mfgtool-linux-imx,i think this is kernel source.
but i don't know how to build the uboot and kernel souce. and don't know where is the target file for build also.
so I see your reply Freescale Technical Information Center
int the uboot chapter.
I see the command.and dont' know where is the <S> ,and what is <package-name>
To Rebuild U-Boot Image:
I try to build uboot
cd ~/yocto
source setup-environment build-x11-mx6qsabresd/
run command bitbake -c compile -f u-boot and get below info
kk@ubuntu:~/y/build-x11-mx6qsabresd$ bitbake -c compile -f u-boot
Parsing recipes: 100% |####################################################################################| Time: 00:00:39
Parsing of 1742 .bb files complete (0 cached, 1742 parsed). 2184 targets, 110 skipped, 1 masked, 0 errors.
ERROR: Nothing PROVIDES 'u-boot'
ERROR: u-boot was skipped: UBOOT_CONFIG emmc is not supported
ERROR: u-boot-imx PROVIDES u-boot but was skipped: UBOOT_CONFIG emmc is not supported
ERROR: u-boot-cubox-i PROVIDES u-boot but was skipped: incompatible with machine imx6qsabresd (not in COMPATIBLE_MACHINE)
ERROR: u-boot-imx PROVIDES u-boot but was skipped: UBOOT_CONFIG emmc is not supported
ERROR: u-boot-congatec PROVIDES u-boot but was skipped: incompatible with machine imx6qsabresd (not in COMPATIBLE_MACHINE)
ERROR: u-boot-boundary PROVIDES u-boot but was skipped: incompatible with machine imx6qsabresd (not in COMPATIBLE_MACHINE)
ERROR: u-boot-fslc PROVIDES u-boot but was skipped: UBOOT_CONFIG emmc is not supported
ERROR: u-boot-imx PROVIDES u-boot but was skipped: You cannot use UBOOT_MACHINE and UBOOT_CONFIG at the same time.
ERROR: u-boot-timesys PROVIDES u-boot but was skipped: incompatible with machine imx6qsabresd (not in COMPATIBLE_MACHINE)
Summary: There was 1 ERROR message shown, returning a non-zero exit code.
I think this is useful for you
The Yocto Project™ and Linux® Software Development for i.MX Application Processors
On page 72 for the details of MFGtool
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi jimmy
thanks for your reply,it's my need.
Really good,thanks again.