hi everyone.
I am working on imx6qp sabre ai board with yocto version Jethro(2.0.1) and Linux kernel 4.1.15.
Now we are working on I-Pod/phone connection for which we procured MFI module(Apple authentication module) from the apple.
As schematics says this module is accommodated at j46. but the device is not detected in the kernel logs as well system.
Can someone help us how to proceed further..?
Regards,
Lavakumar S
hi igorpadykov
thanks for your help i received Patch.
Apple authentication module not detected on the board (IMX6qp sabre AI board) .
Can you help how to dig?
Regards,
Lavakumar S
Thanks for your quick response.
does the driver will detect the MFI module itself ? or do we need to tweek something?
because if i use "i2cdetect -y 1" or "i2cdetect -y 2" i cant see the authentication device address though the MFI module (P/N:sp000918596)connected to j46 .
I am getting proper voltages in the j46 pins i.e pin1 : clock; pin2:Gnd pin3: pulled up pin5: 3.3V pin8: pulled up.
and i have connected the iphone to usb hub and checked (usb connected to USB1 j30).
check and help
Regards,
Lavakumar S
Hi Lavakumar
there is no mfi support in official nxp bsps, suggest to
apply to extended support using NXP Professional Services:
http://www.nxp.com/support/nxp-professional-services:PROFESSIONAL-SERVICE
Best regards
igor
Hi Lavakumar
please create service request to obtain patch.
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Lavakumar
How to create service request :
https://community.freescale.com/docs/DOC-329745
Best regards
igor