I want to work SDMA with EIM on iMX6, but i didn't found that
anyone knows?
I'm using linux kernel 3.0.15
Solved! Go to Solution.
OK, we only have one way : using SW to start SDMA.
Let me see how to !
Customers can send me email to ask for example code on how to use SDMA on WEIM interface !
At same time , Please provide project information.
Email : weidong.sun@freescale.com
Hello Weidong, send me the example code SDMA and EIM dma mem transfer.
My email: fhx9999@163.com
Thanks!!!
Hi weidong:
We need to transfer data over eim from fpga to imx6q processor.
Can you send me the example code for SDMA?
Hello Weidong, send me the example code SDMA and EIM dma mem transfer.
My email: dubovkin.as@gmail.com
Dear Weidong:
I also want to test the mem to mem transfer using SDMA, Could you please send me the example code.
My email: jasper.nuytten@basalte.be
thanks a lot!
Weidong Sun
你好 我是一个中国学生,你我现在在做一个项目会用到EMI接口和FPGA通信,打算采用DMA通信的方式,但是现在遇到一个问题,在测试的时候总线上没有任何信号发生,希望你能发给我一个例程,非常感谢。我的邮箱是bujigr@163.com
郭瑞
Hello Weidong,
I want use SDMA replace memcpy.
please send the examples to me too.
I'm using linux kernel 3.0.35.
my email:liangweilin@nearbylink.com
Thanks!
Hi Weidong Sun,
I would like to know if you can send me an exemple of SDMA and EIM at aurelien.grange@rsautomation.com
Does someone know hox to set EIM clock at 104MHz (to perform SDMA)?
Thanks
Hi Weidong:
could you please send me a copy of MEM TO MEM sdma codes to sales.edgepbx@gmail.com
Thank you very much
Hi Weidong:
Could you please send me a copy of MEM TO MEM SDMA code to rziemins@lgsinnovations.com
Thank you very much
Dear Weidong:
I also want to test the mem to mem transfer using SDMA, Could you please send me the example code.
My email: garam308@gmail.com
thanks a lot!
Dear Weidong:
I also want to test the mem to mem transfer using SDMA, Could you please send me the example code.
My email: lijian@tigergroup.cn
thanks a lot!
Hello,All,
Those friends who recieved Email on WEIM mem to mem help me to press correct answer button !
Thanks
weidong
Hi Weidong,
Can you please send me the example code for SDMA for MEM to MEM transfer?
I'm using the linux version : linux-3.0.35
My mail id :togw2001@yahoo.co.jp
Regards,
Toshiaki Ogawa
Dear Weidong:
I also want to test the mem to mem transfer using SDMA, Could you please send me the example code.
My email: hyunjaiyaa@naver.com
thanks a lot!
Hi Weidong,
I would appreicate if if you could forward the sample code to me.
regards
Pat
Hi Weidong,
Could you also send the sample code to me too?
My email is: stevolution84@gmail.com
Thanks!
Dear Weidong,
Could you also send the sample code to me?
Thanks!
Regards,
Song_Lin