why can't play any format video with hardware decode?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

why can't play any format video with hardware decode?

ソリューションへジャンプ
975件の閲覧回数
Eason_Lian
Contributor II

Hi i.MX Community,

Use source code of fsl-release-bsp-imx-3.10.17-1.0.0_ga,failed play video through command "gplay akiyo.mp4" (example: /unittest/akiyo.mp4).Can you tell me how to resovle it?

BTW,If use mplayer tool,that playing ok.

Refer to imx6q_sabresd board.

Thanks!

Best Regards

Eason

ラベル(4)
タグ(2)
1 解決策
896件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Eason

please try latest BSP

L3.14.28_1.0.0_iMX6QDLS_BUNDLE : i.MX 6Quad, i.MX 6Dual, i.MX 6DualLite, i.MX 6Solo

Linux Binary Demo Files and Linux BSP Documentation 

Size (K): 1479000 Format: gz Rev #: L3.14.28_1.0.0 Modified: 4/10/2015


3.10.17 is removed from i.MX6QD official product web page, so it is not more supported


i.MX6Q|i.MX 6Quad Processors|Quad Core|Freescale

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

2 返答(返信)
897件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Eason

please try latest BSP

L3.14.28_1.0.0_iMX6QDLS_BUNDLE : i.MX 6Quad, i.MX 6Dual, i.MX 6DualLite, i.MX 6Solo

Linux Binary Demo Files and Linux BSP Documentation 

Size (K): 1479000 Format: gz Rev #: L3.14.28_1.0.0 Modified: 4/10/2015


3.10.17 is removed from i.MX6QD official product web page, so it is not more supported


i.MX6Q|i.MX 6Quad Processors|Quad Core|Freescale

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

896件の閲覧回数
Eason_Lian
Contributor II

Hi igor

Thanks for your rapid reply!I'll try it soon.

Best Regards

Eason

0 件の賞賛
返信