what are the pins to be connected in schematic for giving a provision for boot from Nand flash/ SD Card / Internal memory

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

what are the pins to be connected in schematic for giving a provision for boot from Nand flash/ SD Card / Internal memory

761 次查看
muralikrishna
Contributor I

In I.MX6 Quad processor, what are hardware pins to be used in the schematic for selecting boot options from NAND Flash / SD Card / Internal.

标签 (1)
0 项奖励
回复
1 回复

660 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Murali

please look at SPF-27142  p.3, 9

i.MX6_SABRE_AI_DESIGNFILES

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复