Hello,
I haven't found web browser in my imx6 yocto image.
Maybe I missed something ?
If not - is there a suggestion for any simple web browser which I can add ? I've tried to add chromium, but becuase my build system is 32, I get "exhausted memory" error, so I probably better try add other browser.
Thank you,
Ran
已解决! 转到解答。
as stated in sect.5.6.6 :
The Yocto Project community has chromium-imx recipes to enable hardware acceleration
for X11, XWayland, and Wayland version Chromium Browser for i.MX SoC with GPU hardware.
Note that NXP does not support or test the patches from the community, neither for VPU or GPU support.
and this may be posted on meta-fsl-arm mailing list, so that someone familiar with it could try to assist you.
https://lists.yoctoproject.org/listinfo/meta-freescale
Best regards
igor
Hi Ran
supported browsers are described in sect.5.6.6 Chromium Browser on X11, XWayland, and Wayland,
sect.5.6.7 Qt 5 and QtWebEngine browsers attached Yocto Guide
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Thanks,
But for some reason , although there are examples in qt5 , there is no webenginewidgets directory in .../qt5/examples.
And chromium does not build on 32-bit machine because of "exhaused memory".
Thanks,
Ran
as stated in sect.5.6.6 :
The Yocto Project community has chromium-imx recipes to enable hardware acceleration
for X11, XWayland, and Wayland version Chromium Browser for i.MX SoC with GPU hardware.
Note that NXP does not support or test the patches from the community, neither for VPU or GPU support.
and this may be posted on meta-fsl-arm mailing list, so that someone familiar with it could try to assist you.
https://lists.yoctoproject.org/listinfo/meta-freescale
Best regards
igor