Hello,
I am using i.MX6DLSABRE_AI and flashed 5.10.72-2.2.3 BSP files, it is booting up there is no issue. My doubt is i can see only the terminal window in the HDMI monitor (see attachement), is that only option available in this BSP files? or something i have missed? how the windows look like in this version?
To enable frame buffer i have used below command in boot environment "setenv mmcargs 'setenv bootargs console=${console},${baudrate} root=/dev/mmcblk2p2 rootwait rw video=mxcfb0:dev=hdmi,1920x1080M@60,if=RGB24'"
Could you please support me.
did you use prebuit images? if yes, which image do you use?
i have used latest BSP from NXP website as mentioned below:
this demo images are built wayland as backend, if you need other backend, you need build by yourself, more detailed information, pls refer to the ycoto user guide