uuu stuck on 99%

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

uuu stuck on 99%

2,074 次查看
allonli
Contributor II

IMX8MPLUS platform

DDR stress test pass successfully.

build flash.bin standalone

"uuu.exe -b emmc flash.bin" stuck on 99%, UART no log output.

is there any debug method for such situation? 

0 项奖励
回复
7 回复数

2,070 次查看
allonli
Contributor II

ps:add -V parameters, it show error below:

99%libusb: error [windows_transfer_callback] detected I/O error 1167: [1167] 设备没有连接。
1:11>Okay (1.libusb: warning [winusb_get_device_list] could not detect installation state of driver for 'USB\VID_1FC9&PID_0146\6&17382A9&0&1': [3758096907] 设备实例不在硬件树中。

0 项奖励
回复

2,064 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Allon

 

one can recheck if uuu version is compatible with flash.bin,

recommended uuu version is described in Release Notes document of each bsp:

https://www.nxp.com/design/software/embedded-software/i-mx-software/embedded-linux-for-i-mx-applicat...

 

Best regards
igor

0 项奖励
回复

2,056 次查看
allonli
Contributor II

Hi,Igor,

  yes, I use the uuu version as release note described, but same erro.

libusb: error [windows_transfer_callback] detected I/O error 1167: [1167] 设备没有连接。

 

0 项奖励
回复

2,043 次查看
igorpadykov
NXP Employee
NXP Employee

one can try on other computer.

 

Best regards
igor

0 项奖励
回复

2,038 次查看
allonli
Contributor II

yes, have tried.

and also test under Ubuntu system, the same result, but no "winusb" error message even add -V option, just stuck on 99%.

0 项奖励
回复

2,031 次查看
igorpadykov
NXP Employee
NXP Employee

could you try to reproduce issue on i.MX8M Plus EVK.

 

Best regards
igor

 

 

0 项奖励
回复

2,005 次查看
allonli
Contributor II

Hi, Igor,

Sorry,It should not be a uuu tools issue, cannt reproduce on EVK.

It may be customerize hardware or software problem, when stuck here, what's the possible problem, or how to debug it?

thanks a lot.

0 项奖励
回复