u-boot.imx and SPL IMX6UL

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

u-boot.imx and SPL IMX6UL

5,052 Views
omar_aberkan
Contributor III

Is is possible to use u-boot.imx and SPL at the same time? I tried it many times but it failed.

When i use u-boot-ivt.img instead of u-boot.imx everything works fine (signed u-boot-ivt.img + signed SPL).

My question is actually what image do i need for hab encryption and why can't i combine u-boot.imx+ SPL

Comparison:

cat u-boot-ivt.img.log
Image Name:   U-Boot 2019.01-rc1-00780-g0371a0
Created:      Wed Jan 16 21:23:34 2019
Image Type:   ARM U-Boot Firmware with HABv4 IVT (uncompressed)
Data Size:    462784 Bytes = 451.94 KiB = 0.44 MiB
Load Address: 17800000
Entry Point:  00000000
HAB Blocks:   0x177fffc0   0x0000   0x0006f020

cat u-boot.imx.log
Image Type:   Freescale IMX Boot Image
Image Ver:    2 (i.MX53/6/7 compatible)
Mode:         DCD
Data Size:    466944 Bytes = 456.00 KiB = 0.45 MiB
Load Address: 177ff420
Entry Point:  17800000
HAB Blocks:   0x177ff400 0x00000000 0x0006fc00
DCD Blocks:   0x00910000 0x0000002c 0x00000004

As you can see the Entry point for u-boot-ivt.img is 00000000 and there are no DCD blocks, if i am not wrong in need

those values to the encryption.

I hope somebody can help me out.

2.8.0.0 i
0 Kudos
Reply
3 Replies

3,610 Views
igorpadykov
NXP Employee
NXP Employee

Hi Omar

nxp does not support i.MX6UL SPL  in its releases, may be useful

to check third party tutorial about i.MX6 SPL boot

ventana/bootloader – Gateworks 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

3,610 Views
omar_aberkan
Contributor III

Where can i find the releases from nxp? I used the bsp from meta-freescale to build my images. How can i install u-boot.imx on the imx6ulevk?

0 Kudos
Reply

3,610 Views
igorpadykov
NXP Employee
NXP Employee

nxp releases link:

uboot-imx - i.MX U-Boot 

documentation

i.MX Software|NXP 

Best regards
igor

0 Kudos
Reply