the interval of the reading data through IIC1 is too long

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

the interval of the reading data through IIC1 is too long

816件の閲覧回数
zhanghan
Contributor II

QQ图片20171128164301.png

I use imx6 IIC1 to monitor my power,but i find the interval between every twice data is 1.6s,because when power off ,the ch1 is power off  before system 3.3V power 300ms ,so I want to get the chI data  during the 300ms.then I can determine whether the voltage of ch1 is lower , but now the interval between every  two times of data is 1.6s,so Most of the time I can't get data,rare time i can get the data 。during the last pic ,the yellow line is SCL of IIC,the blue is the voltage of 

CH1 。the interval of the cusor is 1.6s approximately。can somebody tell me how to reduce the 1.6s。is it related with Kernel?

1.png3.jpg

ラベル(1)
0 件の賞賛
返信
3 返答(返信)

759件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi zhang

long interval may be due to printfs, also one can try to run application on separate core.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

759件の閲覧回数
zhanghan
Contributor II

Can you tell me more detail?what does “ one can try to run application on separate core”mean?

0 件の賞賛
返信

759件の閲覧回数
igorpadykov
NXP Employee
NXP Employee
0 件の賞賛
返信