stop here while download android6.0.1_2 image with emmc

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

stop here while download android6.0.1_2 image with emmc

1,679 Views
jiejia
Contributor III

I want to download the android M6 image files in emmc on my board reference imx6q sabresd.

I have downloaded the following files.

・android_M6.0.1_2.0.0_image_6dqpsabresd.tar.gz

・android_m6.0.1_2.0.0_ga_tool.tar.gz

I referred the android_M6.0.1_2.0.0_docs/Android_User's_Guide.pdf, Getting Android source code(Android/kernel/u-boot) and then building Android images. As my board has no pmic, I delete the contents about pmic in u-boot.

I copy u-boot.imx to \mfgtools_m6.0.1_1.0.0_ga\Profiles\Linux\OS Firmware\firmware and replace to old one (u-boot-imx6qsabresd_sd.imx). Then open MFGTool to download image. I can enter u-boot command line, but it stop here.

U-Boot 2015.04-14490-g596b7a8-dirty (Aug 18 2016 - 14:18:35)

CPU:   Freescale i.MX6Q rev1.5 at 792 MHz

CPU:   Temperature 30 C

Reset cause: POR

Board: MX6-SabreSD

I2C:   ready

DRAM:  1 GiB

MMC:   FSL_SDHC: 0, FSL_SDHC: 1, FSL_SDHC: 2

*** Warning - bad CRC, using default environment

No panel detected: default to Hannstar-XGA

Display: Hannstar-XGA (1024x768)

In:    serial

Out:   serial

Err:   serial

switch to partitions #0, OK

mmc2(part 0) is current device

check_and_clean: reg 0, flag_set 0

Cannot find partition 8

rw_block, get_block_size return 0

read_bootctl, rw_block read failed

read command failed

Fastboot: Normal

flash target is MMC:2

Bad partition index:1 for partition:boot

Bad partition index:2 for partition:recovery

Bad partition index:5 for partition:system

Bad partition index:4 for partition:data

Net:   FEC [PRIME]

Error: FEC address not set.

Boot from USB for mfgtools

Use default environment for                              mfgtools

Run bootcmd_mfg: run mfgtool_args;bootz ${loadaddr} ${initrd_addr} ${fdt_addr};

Hit any key to stop autoboot:  0

Kernel image @ 0x12000000 [ 0x000000 - 0x552a48 ]

## Loading init Ramdisk from Legacy Image at 12c00000 ...

   Image Name:   fsl-image-mfgtool-initramfs-imx6

   Image Type:   ARM Linux RAMDisk Image (gzip compressed)

   Data Size:    7565864 Bytes = 7.2 MiB

   Load Address: 00000000

   Entry Point:  00000000

   Verifying Checksum ... OK

## Flattened Device Tree blob at 18000000

   Booting using the fdt blob at 0x18000000

   Using Device Tree in place at 18000000, end 1800e197

No PMIC found!

Starting kernel ...

Booting Linux on physical CPU 0x0

Linux version 4.1.15-1.0.0-mfgtool+g3924425 (bamboo@shlinux12) (gcc version 5.2.0 (GCC) ) #1 SMP PREEMPT Sun Mar 13 17:19:17 CST 2016

CPU: ARMv7 Processor [412fc09a] revision 10 (ARMv7), cr=10c5387d

CPU: PIPT / VIPT nonaliasing data cache, VIPT aliasing instruction cache

Machine model: Freescale i.MX6 Quad SABRE Smart Device Board

Reserved memory: created CMA memory pool at 0x3c000000, size 320 MiB

Reserved memory: initialized node linux,cma, compatible id shared-dma-pool

Memory policy: Data cache writealloc

PERCPU: Embedded 12 pages/cpu @ab705000 s16768 r8192 d24192 u49152

Built 1 zonelists in Zone order, mobility grouping on.  Total pages: 260096

Kernel command line: console=ttymxc0,115200 rdinit=/linuxrc g_mass_storage.stall=0 g_mass_storage.removable=1 g_mass_storage.file=/fat g_mass_storage.ro=1 g_mass_storage.idVendor=0x066F g_mass_storage.idProduct=0x37FF g_mass_storage.iSerialNumber= enable_wait_mode=off

PID hash table entries: 4096 (order: 2, 16384 bytes)

Dentry cache hash table entries: 131072 (order: 7, 524288 bytes)

Inode-cache hash table entries: 65536 (order: 6, 262144 bytes)

Memory: 693016K/1048576K available (6895K kernel code, 319K rwdata, 2412K rodata, 388K init, 423K bss, 27880K reserved, 327680K cma-reserved, 0K highmem)

Virtual kernel memory layout:

    vector  : 0xffff0000 - 0xffff1000   (   4 kB)

    fixmap  : 0xffc00000 - 0xfff00000   (3072 kB)

    vmalloc : 0xc0800000 - 0xff000000   (1000 MB)

    lowmem  : 0x80000000 - 0xc0000000   (1024 MB)

    pkmap   : 0x7fe00000 - 0x80000000   (   2 MB)

    modules : 0x7f000000 - 0x7fe00000   (  14 MB)

      .text : 0x80008000 - 0x8091ef88   (9308 kB)

      .init : 0x8091f000 - 0x80980000   ( 388 kB)

      .data : 0x80980000 - 0x809cff00   ( 320 kB)

       .bss : 0x809d2000 - 0x80a3bf14   ( 424 kB)

SLUB: HWalign=64, Order=0-3, MinObjects=0, CPUs=4, Nodes=1

Preemptible hierarchical RCU implementation.

        Additional per-CPU info printed with stalls.

NR_IRQS:16 nr_irqs:16 16

L2C-310 erratum 769419 enabled

L2C-310 enabling early BRESP for Cortex-A9

L2C-310 full line of zeros enabled for Cortex-A9

L2C-310 ID prefetch enabled, offset 16 lines

L2C-310 dynamic clock gating enabled, standby mode enabled

L2C-310 cache controller enabled, 16 ways, 1024 kB

L2C-310: CACHE_ID 0x410000c7, AUX_CTRL 0x76070001

mxc_clocksource_init 3000000

Switching to timer-based delay loop, resolution 333ns

sched_clock: 32 bits at 3000kHz, resolution 333ns, wraps every 715827882841ns

clocksource mxc_timer1: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 637086815595 ns

Console: colour dummy device 80x30

Calibrating delay loop (skipped), value calculated using timer frequency.. 6.00 BogoMIPS (lpj=30000)

pid_max: default: 32768 minimum: 301

Mount-cache hash table entries: 2048 (order: 1, 8192 bytes)

Mountpoint-cache hash table entries: 2048 (order: 1, 8192 bytes)

CPU: Testing write buffer coherency: ok

CPU0: thread -1, cpu 0, socket 0, mpidr 80000000

Setting up static identity map for 0x10008280 - 0x100082f0

CPU1: thread -1, cpu 1, socket 0, mpidr 80000001

CPU2: thread -1, cpu 2, socket 0, mpidr 80000002

CPU3: thread -1, cpu 3, socket 0, mpidr 80000003

Brought up 4 CPUs

SMP: Total of 4 processors activated (24.00 BogoMIPS).

CPU: All CPU(s) started in SVC mode.

devtmpfs: initialized

VFP support v0.3: implementor 41 architecture 3 part 30 variant 9 rev 4

clocksource jiffies: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 19112604462750000 ns

pinctrl core: initialized pinctrl subsystem

NET: Registered protocol family 16

DMA: preallocated 256 KiB pool for atomic coherent allocations

cpuidle: using governor ladder

cpuidle: using governor menu

CPU identified as i.MX6Q, silicon rev 1.5

hw-breakpoint: found 5 (+1 reserved) breakpoint and 1 watchpoint registers.

hw-breakpoint: maximum watchpoint size is 4 bytes.

imx6q-pinctrl 20e0000.iomuxc: initialized IMX pinctrl driver

mxs-dma 110000.dma-apbh: initialized

SCSI subsystem initialized

usbcore: registered new interface driver usbfs

usbcore: registered new interface driver hub

usbcore: registered new device driver usb

2000000.aips-bus:usbphy_nop1 supply vcc not found, using dummy regulator

2000000.aips-bus:usbphy_nop2 supply vcc not found, using dummy regulator

i2c i2c-0: IMX I2C adapter registered

i2c i2c-0: can't use DMA

i2c i2c-1: IMX I2C adapter registered

i2c i2c-1: can't use DMA

i2c i2c-2: IMX I2C adapter registered

i2c i2c-2: can't use DMA

Linux video capture interface: v2.00

pps_core: LinuxPPS API ver. 1 registered

pps_core: Software ver. 5.3.6 - Copyright 2005-2007 Rodolfo Giometti <giometti@linux.it>

PTP clock support registered

imx-ipuv3 2400000.ipu: IPU DMFC NORMAL mode: 1(0~1), 5B(4,5), 5F(6,7)

imx-ipuv3 2800000.ipu: IPU DMFC NORMAL mode: 1(0~1), 5B(4,5), 5F(6,7)

Advanced Linux Sound Architecture Driver Initialized.

Switched to clocksource mxc_timer1

NET: Registered protocol family 2

TCP established hash table entries: 8192 (order: 3, 32768 bytes)

TCP bind hash table entries: 8192 (order: 4, 65536 bytes)

TCP: Hash tables configured (established 8192 bind 8192)

UDP hash table entries: 512 (order: 2, 16384 bytes)

UDP-Lite hash table entries: 512 (order: 2, 16384 bytes)

NET: Registered protocol family 1

RPC: Registered named UNIX socket transport module.

RPC: Registered udp transport module.

RPC: Registered tcp transport module.

RPC: Registered tcp NFSv4.1 backchannel transport module.

Trying to unpack rootfs image as initramfs...

Freeing initrd memory: 7392K (82c00000 - 83338000)

CPU PMU: Failed to parse /soc/pmu/interrupt-affinity[0]

hw perfevents: enabled with armv7_cortex_a9 PMU driver, 7 counters available

imx rpmsg driver is registered.

Bus freq driver module loaded

futex hash table entries: 1024 (order: 4, 65536 bytes)

VFS: Disk quotas dquot_6.6.0

VFS: Dquot-cache hash table entries: 1024 (order 0, 4096 bytes)

NFS: Registering the id_resolver key type

Key type id_resolver registered

Key type id_legacy registered

jffs2: version 2.2. (NAND) 漏 2001-2006 Red Hat, Inc.

fuse init (API version 7.23)

io scheduler noop registered

io scheduler deadline registered

io scheduler cfq registered (default)

imx-weim 21b8000.weim: Driver registered.

backlight supply power not found, using dummy regulator

mxc_sdc_fb fb@0: NO mxc display driver found!

mxc_sdc_fb fb@1: NO mxc display driver found!

mxc_sdc_fb fb@2: registered mxc display driver lcd

Console: switching to colour frame buffer device 100x30

mxc_sdc_fb fb@3: NO mxc display driver found!

imx-sdma 20ec000.sdma: no iram assigned, using external mem

imx-sdma 20ec000.sdma: no event needs to be remapped

imx-sdma 20ec000.sdma: loaded firmware 3.3

imx-sdma 20ec000.sdma: initialized

pfuze100-regulator 1-0008: unrecognized pfuze chip ID!

pfuze100-regulator: probe of 1-0008 failed with error -5

2020000.serial: ttymxc0 at MMIO 0x2020000 (irq = 25, base_baud = 5000000) is a IMX

console [ttymxc0] enabled

imx sema4 driver is registered.

[drm] Initialized drm 1.1.0 20060810

[drm] Initialized vivante 1.0.0 20120216 on minor 0

brd: module loaded

loop: module loaded

ahci-imx 2200000.sata: fsl,transmit-level-mV not specified, using 00000024

ahci-imx 2200000.sata: fsl,transmit-boost-mdB not specified, using 00000480

ahci-imx 2200000.sata: fsl,transmit-atten-16ths not specified, using 00002000

ahci-imx 2200000.sata: fsl,receive-eq-mdB not specified, using 05000000

ahci-imx 2200000.sata: SSS flag set, parallel bus scan disabled

ahci-imx 2200000.sata: AHCI 0001.0300 32 slots 1 ports 3 Gbps 0x1 impl platform mode

ahci-imx 2200000.sata: flags: ncq sntf stag pm led clo only pmp pio slum part ccc apst

scsi host0: ahci-imx

ata1: SATA max UDMA/133 mmio [mem 0x02200000-0x02203fff] port 0x100 irq 309

m25p80 spi0.0: unrecognized JEDEC id bytes: 00,  0,  0

spi_imx 2008000.ecspi: probed

2188000.ethernet supply phy not found, using dummy regulator

pps pps0: new PPS source ptp0

fec 2188000.ethernet (unnamed net_device) (uninitialized): Invalid MAC address: 00:00:00:00:00:00

fec 2188000.ethernet (unnamed net_device) (uninitialized): Using random MAC address: 0a:27:62:82:57:21

libphy: fec_enet_mii_bus: probed

fec 2188000.ethernet eth0: registered PHC device 0

ehci_hcd: USB 2.0 'Enhanced' Host Controller (EHCI) Driver

ehci-mxc: Freescale On-Chip EHCI Host driver

usbcore: registered new interface driver usb-storage

2184800.usbmisc supply vbus-wakeup not found, using dummy regulator

reg-fixed-voltage regulators:regulator@0: Failed to resolve vin-supply for usb_otg_vbus

imx_usb 2184000.usb: Can't register ci_hdrc platform device, err=-517

reg-fixed-voltage regulators:regulator@1: Failed to resolve vin-supply for usb_h1_vbus

imx_usb 2184200.usb: Can't register ci_hdrc platform device, err=-517

udc-core: couldn't find an available UDC - added [g_mass_storage] to list of pending drivers

mousedev: PS/2 mouse device common for all mice

egalax_ts 1-0004: Failed to read firmware version

egalax_ts: probe of 1-0004 failed with error -5

egalax_ts 2-0004: Failed to read firmware version

egalax_ts: probe of 2-0004 failed with error -5

snvs_rtc 20cc000.snvs:snvs-rtc-lp: rtc core: registered 20cc000.snvs:snvs-r as rtc0

i2c /dev entries driver

IR NEC protocol handler initialized

IR RC5(x/sz) protocol handler initialized

IR RC6 protocol handler initialized

IR JVC protocol handler initialized

IR Sony protocol handler initialized

IR SANYO protocol handler initialized

IR Sharp protocol handler initialized

IR MCE Keyboard/mouse protocol handler initialized

IR XMP protocol handler initialized

imx2-wdt 20c0000.wdog: use WDOG_B to reboot.

imx2-wdt 20c0000.wdog: timeout 60 sec (nowayout=0)

sdhci: Secure Digital Host Controller Interface driver

sdhci: Copyright(c) Pierre Ossman

sdhci-pltfm: SDHCI platform and OF driver helper

/soc/aips-bus@02100000/usdhc@02194000: voltage-ranges unspecified

sdhci-esdhc-imx 2194000.usdhc: Got CD GPIO

sdhci-esdhc-imx 2194000.usdhc: Got WP GPIO

sdhci-esdhc-imx 2194000.usdhc: No vmmc regulator found

sdhci-esdhc-imx 2194000.usdhc: No vqmmc regulator found

mmc1: SDHCI controller on 2194000.usdhc [2194000.usdhc] using ADMA

/soc/aips-bus@02100000/usdhc@02198000: voltage-ranges unspecified

sdhci-esdhc-imx 2198000.usdhc: Got CD GPIO

sdhci-esdhc-imx 2198000.usdhc: Got WP GPIO

sdhci-esdhc-imx 2198000.usdhc: No vmmc regulator found

sdhci-esdhc-imx 2198000.usdhc: No vqmmc regulator found

ata1: SATA link down (SStatus 0 SControl 300)

ahci-imx 2200000.sata: no device found, disabling link.

ahci-imx 2200000.sata: pass ahci_imx..hotplug=1 to enable hotplug

mmc2: SDHCI controller on 2198000.usdhc [2198000.usdhc] using ADMA

/soc/aips-bus@02100000/usdhc@0219c000: voltage-ranges unspecified

sdhci-esdhc-imx 219c000.usdhc: No vmmc regulator found

sdhci-esdhc-imx 219c000.usdhc: No vqmmc regulator found

mmc3: SDHCI controller on 219c000.usdhc [219c000.usdhc] using ADMA

mxc_vpu 2040000.vpu_fsl: VPU initialized

mxc_vdoa 21e4000.vdoa: i.MX Video Data Order Adapter(VDOA) driver probed

usbcore: registered new interface driver usbhid

usbhid: USB HID core driver

wm8962 0-001a: Failed to read ID register

wm8962: probe of 0-001a failed with error -5

imx-wm8962 sound: failed to find codec platform device

imx-wm8962: probe of sound failed with error -22

NET: Registered protocol family 10

sit: IPv6 over IPv4 tunneling driver

NET: Registered protocol family 17

Key type dns_resolver registered

cpu cpu0: failed to get regulators

imx6q-cpufreq: probe of imx6q-cpufreq.0 failed with error -2

Registering SWP/SWPB emulation handler

mmc3: new DDR MMC card at address 0001

mmcblk3: mmc3:0001 SEM08G 7.39 GiB

mmcblk3boot0: mmc3:0001 SEM08G partition 1 1.00 MiB

mmcblk3boot1: mmc3:0001 SEM08G partition 2 1.00 MiB

mmcblk3rpmb: mmc3:0001 SEM08G partition 3 128 KiB

reg-fixed-voltage regulators:regulator@0: Failed to resolve vin-supply for usb_otg_vbus

imx_usb 2184000.usb: Can't register ci_hdrc platform device, err=-517

reg-fixed-voltage regulators:regulator@1: Failed to resolve vin-supply for usb_h1_vbus

imx_usb 2184200.usb: Can't register ci_hdrc platform device, err=-517

input: gpio-keys as /devices/soc0/gpio-keys/input/input2

snvs_rtc 20cc000.snvs:snvs-rtc-lp: setting system clock to 1970-01-01 00:00:00 UTC (0)

reg-fixed-voltage regulators:regulator@0: Failed to resolve vin-supply for usb_otg_vbus

imx_usb 2184000.usb: Can't register ci_hdrc platform device, err=-517

reg-fixed-voltage regulators:regulator@1: Failed to resolve vin-supply for usb_h1_vbus

imx_usb 2184200.usb: Can't register ci_hdrc platform device, err=-517

mipi_dsi_pwr_on: disabling

sensor-supply: disabling

wm8962-supply: disabling

usb_h1_vbus: disabling

usb_otg_vbus: disabling

ALSA device list:

  No soundcards found.

Freeing unused kernel memory: 388K (8091f000 - 80980000)

Starting UTP

uuc 0.5 [built Mar 12 2016 19:04:20]

UTP: Waiting for device to appear

random: nonblocking pool is initialized

0 Kudos
Reply
4 Replies

1,016 Views
igorpadykov
NXP Employee
NXP Employee

Hi jie

as board has not pmic please delete the contents about pmic in linux too,

please refer to attached Linux Manual. (Android is based on LInux).

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

1,015 Views
femb_niuyi
Contributor I

Hi igorpadykov

Please, How can I delete PMIC from Linux? I don't see the instructions in the manual(i.MX_Linux_Reference_Manual.pdf). Can you describe it in detail?

Thank you.

Best regards.

Niuyi

0 Kudos
Reply

1,015 Views
igorpadykov
NXP Employee
NXP Employee

Hi Niuyi

in theory it can be deleted, but I think it is not easy as it is integrated in many drivers.

NXP does not provide documentation for that, sorry.

Best regards
igor

0 Kudos
Reply

1,016 Views
femb_niuyi
Contributor I

Hi igor

After many attempts, I solved this problem. Thank you.

Bast regards.

niuyi

0 Kudos
Reply