Hi all
It is a question for the reference design.
Schematic file name: SPF-28616_C2.pdf
Target page: page 12
As a result of checking the circuit, the signal for controlling the power supply (SD_VDD) to the SD slot was added to SD1_nRST and POR_B.
Could you tell us why you need POR_B for SD power control ?
Ko-hey
Hello,
The POR_B provides also SD card and interface reset so that both i.MX6 and SD card
were in predefined (after reset) state. This allows to avoid issues when SD continues its
previous operation during attempts of i.MX6 to initialize SD (eMMC).
Also, please take a look at https://community.nxp.com/message/469357
Have a great day,
Yuri
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------