remote control with Wayland/Weston support (Yocto)

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

remote control with Wayland/Weston support (Yocto)

5,966件の閲覧回数
shai_b
Senior Contributor II

Dear Team,

My customer is looking to have a remote control ability with Wayland/Weston support.

Can you please suggest a method to control Linux (Yocto) such as anydesk?

Waiting for your kind feedback, many thanks.

Kind regards,

Shai 

タグ(1)
0 件の賞賛
返信
8 返答(返信)

4,877件の閲覧回数
prashantdivate
Contributor II

Hi @shai_b and @Sanket_Parekh 

I was recently working on same use case and I succeeded in remotely access Wayland application using the RDP client in yocto environment. All the steps I captured in my blog hopefully it will be helpful for you


FYI- 
full article
https://medium.com/@prashant-divate/remotely-accessing-wayland-based-applications-using-rdp-client-i...

addressed in meta layer
https://github.com/prashantdivate/meta-sirius/tree/master

0 件の賞賛
返信

5,950件の閲覧回数
Sanket_Parekh
NXP TechSupport
NXP TechSupport

Hello @shai_b 

I hope you are doing well.

->Yes, one can control Linux from another PC.

1)Through CLI:-
->One can remotely work on another pc if both pc is connected to the same network.
->one can use SSH utility for the same.
ssh user_name@host(IP/Domain_name)

2) Through GUI:-
->One can use the Weston-RDP app for the same.
->One can refer to this RDP (remote desktop protocol).

Thanks & Regards.

Sanket Parekh

5,942件の閲覧回数
shai_b
Senior Contributor II

@Sanket_Parekh Hello,

Thank you so much for your details responses.

Can you please advise if the default iMX BSP includes Weston-RDP?

if not what is the procedure to include Weston-RDP into NXP Yocto BSP?

Waiting for your kind feedback, many thanks.

Regards,

Shai

0 件の賞賛
返信

5,925件の閲覧回数
Sanket_Parekh
NXP TechSupport
NXP TechSupport

Hello @shai_b ,

I hope you are doing well.

1)Can you please advise if the default iMX BSP includes Weston-RDP?
->By default BSP doesn't have it included.
->One has to build it separately.

one can refer to the below-given link for reference, there are steps provided to build it.
https://community.nxp.com/t5/i-MX-Processors/i-MX8-How-to-share-screen-on-Weston/td-p/1333875

Thanks & Regards
Sanket Parekh

0 件の賞賛
返信

5,897件の閲覧回数
shai_b
Senior Contributor II

Hi @Sanket_Parekh,

Thanks for your input, I will try to follow them and will advise back if needed.

Thanks again.

Regards,

Shai

0 件の賞賛
返信

5,836件の閲覧回数
Sanket_Parekh
NXP TechSupport
NXP TechSupport
Hello @shai_b ,
 
I hope you are doing well.
 
Any Updates from your side?
 
Thanks & Regards,
Sanket Parekh
0 件の賞賛
返信

5,817件の閲覧回数
shai_b
Senior Contributor II
Hello @Sanket_Parekh ,
The customer still working on this, I will advise you back as needed.
Thank you so much for your support.

Kind regards,
Shai
0 件の賞賛
返信

5,810件の閲覧回数
Sanket_Parekh
NXP TechSupport
NXP TechSupport
Hello @shai_b ,


I hope you are doing well.

->Ok, Please advise back if needed.

Thanks & Regards,

Sanket Parekh