pins state during POR

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

pins state during POR

跳至解决方案
864 次查看
eishishibusawa
Contributor III

Dear Sir

 

I want to ask you about i.MX6ULL.

 

Q1.

I want to know the state of the pins during POR is asserted.

Does it have been described in the manual or data sheet?

 

Best Regards,

Eishi SHIBUSAWA

标签 (1)
0 项奖励
回复
1 解答
730 次查看
Yuri
NXP Employee
NXP Employee

Hello,

  There are pin states, provided in the DataSheet(s), relate to situation just after reset ;

pin states during power on \ reset are not guaranteed.

Regards,

Yuri.

在原帖中查看解决方案

0 项奖励
回复
2 回复数
731 次查看
Yuri
NXP Employee
NXP Employee

Hello,

  There are pin states, provided in the DataSheet(s), relate to situation just after reset ;

pin states during power on \ reset are not guaranteed.

Regards,

Yuri.

0 项奖励
回复
730 次查看
joanxie
NXP TechSupport
NXP TechSupport

refer to the data sheet:

"The SRC_POR_B signal controls the processor POR and must be immediately asserted at
power-up and remain asserted until the VDD_ARM_CAP, VDD_SOC_CAP, and VDD_PU_CAP
supplies are stable. VDD_ARM_IN and VDD_SOC_IN may be applied in either order with no
restrictions."

for more detailed information, pls refer to the Power-Up Sequence of data sheet.

0 项奖励
回复