opp-suspend defined in all imx8mn operating points

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

opp-suspend defined in all imx8mn operating points

519 次查看
moose
Contributor IV

According to Generic OPP Bindings, listing `opp-suspend` property in all operating points will force the one with the highest running clock. In a53_opp_table node defined within imx8mn.dtsi, `opp-suspend` is listed in all operating points. Wouldn't this select the 1.5GHz operating during suspend? If yes, shouldn't `opp-suspend` only be listed within the 1.2GHz point?
 

a53_opp_table: opp-table {
compatible = "operating-points-v2";
opp-shared;
opp-1200000000 {
opp-hz = /bits/ 64 <1200000000>;
opp-microvolt = <850000>;
opp-supported-hw = <0xb00>, <0x7>;
clock-latency-ns = <150000>;
opp-suspend;
};
 
opp-1400000000 {
opp-hz = /bits/ 64 <1400000000>;
opp-microvolt = <950000>;
opp-supported-hw = <0x300>, <0x7>;
clock-latency-ns = <150000>;
opp-suspend;
};
 
opp-1500000000 {
opp-hz = /bits/ 64 <1500000000>;
opp-microvolt = <1000000>;
opp-supported-hw = <0x100>, <0x3>;
clock-latency-ns = <150000>;
opp-suspend;
};
};
标签 (1)
标记 (1)
0 项奖励
回复
3 回复数

504 次查看
joanxie
NXP TechSupport
NXP TechSupport

the driver would change the frequency Dynamically, you don't need change the table by youself

0 项奖励
回复

502 次查看
moose
Contributor IV

Agreed. The question is what frequency would the driver choose in suspend mode. 

0 项奖励
回复

495 次查看
joanxie
NXP TechSupport
NXP TechSupport

for suspend mode, the arm core is power-gated

Suspend mode
This mode is called either Dormant mode or Deep sleep mode in the Linux BSP. This is the lowest possible power state where the external supplies are still on.
The use case is as follows:
• The Arm platform is power-gated.
• The L2 Cache peripherals are power-gated.
• The Arm Cortex-M4 is in the reset status.
• All PLL (Phase-Locked Loop) and CCM (Clock Controller Module) generated clocks are OFF.
• The CKIL (32 kHz) input is on.
• All modules are disabled.
• The external high-frequency crystal and the on-chip oscillator are powered down (by asserting the SBYOS bit in the CCM).

 

0 项奖励
回复