mx6q quard preassembled uboot flashing

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

mx6q quard preassembled uboot flashing

1,855 Views
LLlypukag3e2010
Contributor I

Hi everyone!

Can smb help?

i have a braded unit with ubuntu 13.04 onboard and EOL support from manufacter.

BoardID: MX6Q/SDL-SabreSD. 2GB Ram onboard,

inside is old 2013 uboot without "stop load" function. it flashed to spi separately. partition with uboot mount in system with rw support.

I'm going to flash it by this manual https://boundarydevices.com/programming-emmc-on-i-mx-platforms/ and try pre-compilied ubuntu 18.04

I found uart and connected to console

so here is question:

Is it possible to use pre-assembled uboot for this platform https://boundarydevices.com/wiki/bd-sl-imx6/ (from wiki boundarydevices)  instead of original? i think there are ohther boardid but hardware is identic

0 Kudos
Reply
9 Replies

1,423 Views
rwadraa7
Contributor I

Your blog is great, congratulations on your great work!

0 Kudos
Reply

1,757 Views
humansur
Contributor I
0 Kudos
Reply

1,819 Views
LLlypukag3e2010
Contributor I

it was not the best idea. got brick and waste time for repair. sabre light u-boot even not started on sabresd

0 Kudos
Reply

1,795 Views
igorpadykov
NXP Employee
NXP Employee

provided links were given to make decision: what actual board in hands - Sabre SD or Sabre Lite

(as uboot logs may be misleading). Based on that you can proceed with flashing proper image.

 

Best regards
igor

0 Kudos
Reply

1,847 Views
igorpadykov
NXP Employee
NXP Employee

Hi LLlypukag3e2010

 

one can try, however this manual is for https://boundarydevices.com/wiki/bd-sl-imx6/

board, not NXP "SabreSD", so in general there is chance that it will not work.

 

Best regards
igor

 

0 Kudos
Reply

1,843 Views
LLlypukag3e2010
Contributor I

Hello, Igor. can you try to explain differences between that platforms?

as i see from description - they are almost similiar. main diference -2gb ram in my "SABRESD" instead 1gb in "boundarydevice". oh, one more thing - it's call "SABRE Lite" formerly.

https://boundarydevices.com/sabre-lite-name-change-bd-sl-i-mx6-built-to-freescale-sabre-lite-design/

main reason of question - i couldn't found jtag pins on my board, so in case wrong u-boot device just will be brick. and recover will be possible only with tl866...(

anyway, i'll share result of my experiment.

0 Kudos
Reply

1,769 Views
mpandoayw
Contributor I

Your blog is simply amazing, congratulations on your great work! UPSers

0 Kudos
Reply

1,809 Views
mpandoayw
Contributor I

Thank you so much for sharing such a useful information. I will definitely share this with others. 

0 Kudos
Reply

1,837 Views
igorpadykov
NXP Employee
NXP Employee
0 Kudos
Reply