mx6 Solo and/or DualLight with two cameras (parallel interface)

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

mx6 Solo and/or DualLight with two cameras (parallel interface)

跳至解决方案
1,419 次查看
ilangoodman
Contributor I

Is it possible with either the i.mx6 Solo or Dual Light to connect two cameras using two separate parallel interfaces, and receive the two video streams simultaneously? In this application we are not using any display devices, we just want to get the images / video from both cameras into memory. It's not even entirely clear to me whether the Solo has two parallel interfaces, though it seems that the Dual Light definitely does..

Thanks,

ilan

标签 (4)
0 项奖励
回复
1 解答
876 次查看
Yuri
NXP Employee
NXP Employee

Yes, this is possible. The second CSI port is mux-ed with EIM signals.

在原帖中查看解决方案

0 项奖励
回复
2 回复数
877 次查看
Yuri
NXP Employee
NXP Employee

Yes, this is possible. The second CSI port is mux-ed with EIM signals.

0 项奖励
回复
876 次查看
ilangoodman
Contributor I

Thanks Yuri. We're making an adapter board to add the second parallel interface to the Boundary Devices SABRE Lite board so we can test this.

** FOLLOW UP **

We've now got two OV5642 (10 bit parallel interface) streaming video simultaneously on the SABRE Lite board with DualLite processor. Thanks for your help!

0 项奖励
回复