Hello community,
Is there any tested libmcc available for imx6sx. I tried the driver in the original package but it seems it has some issues. any alternative?
Cheers,
Sina
Hi Sina
latest 3.14.52 BSP includes RPMsg driver, description can be found
in attached Linux Manual Chapter 52.
Board Support Packages (29)
L3.14.52_1.1.0_MX6QDLSOLO (REV L3.14.52_1.1.0)
I am not aware of other mcc libraries.
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hello Igor,
Thanks for the quick replay. Actually we are aware of the RPMsg driver but the point is that we couldn't find any proper RTOS image is used for the Cortex-M4 processor. In the document it is mentioned that the Cortex-M4 processor RTOS should run on the QSPI NOR flash on the i.MX 6SoloX. Is there any RTOS image avaible that we can download for this purpose? Is the driver avaiable on the RTOS side?
Cheers,
Sina