Hi All,
Is there a version of kobs-ng (running 1.2) that supports the dump command on an i.mx6 part? The current code is looking for NCB blocks instead of FCB which looks like it is for other i.mx parts. I have found a few references to this topic for other i.mx processors but none relating to the i.mx6.
Hi Peter,
I tried the kobs-ng you attached on my mx6solo board. After kobs-ng init -v u-boot.bin, kobs-ng dump show fingerprints mismatch:
<<<<
> ./kobs-ng init -v u-boot.bin
MTD CONFIG:
chip_0_device_path = "/dev/mtd0"
chip_1_device_path = "(null)"
search_exponent = 2
data_setup_time = 80
data_hold_time = 60
address_setup_time = 25
data_sample_time = 6
row_address_size = 3
column_address_size = 2
read_command_code1 = 0
read_command_code2 = 48
boot_stream_major_version = 1
boot_stream_minor_version = 0
boot_stream_sub_version = 0
ncb_version = 3
boot_stream_1_address = 0
boot_stream_2_address = 0
u-boot.bin: verifying using key '00000000000000000000000000000000'
u-boot.bin: is a valid bootstream for key '00000000000000000000000000000000'
mtd: opening: "/dev/mtd0"
mtd: '/dev/mtd0' bad block @ 0x1140000 (MTD)
mtd: '/dev/mtd0' bad block @ 0x2b00000 (MTD)
mtd: '/dev/mtd0' bad block @ 0x6380000 (MTD)
mtd: '/dev/mtd0' bad block @ 0x18000000 (MTD)
mtd: '/dev/mtd0' bad block @ 0x18040000 (MTD)
mtd: '/dev/mtd0' bad block @ 0x1ba00000 (MTD)
mtd: '/dev/mtd0' bad block @ 0x261c0000 (MTD)
mtd: '/dev/mtd0' bad block @ 0x26240000 (MTD)
mtd: '/dev/mtd0' bad block @ 0x38000000 (MTD)
mtd: '/dev/mtd0' bad block @ 0x38040000 (MTD)
mtd: '/dev/mtd0' bad block @ 0x3a580000 (MTD)
NFC geometry :
ECC Strength : 8
Page Size in Bytes : 4224
Metadata size : 10
ECC Chunk Size in byte : 512
ECC Chunk count : 8
Block Mark Byte Offset : 3995
Block Mark Bit Offset : 0
====================================================
mtd: opened '/dev/mtd0' - '(null)'
mtd: max_boot_stream_size_in_bytes = 535822336
mtd: boot_stream_size_in_bytes = 214788
mtd: boot_stream_size_in_pages = 53
mtd: #1 0x00200000 - 0x20100000 (0x00234704)
mtd: #2 0x20100000 - 0x40000000 (0x20134704)
FCB
m_u32Checksum = 0x00000000
m_u32FingerPrint = 0x20424346
m_u32Version = 0x01000000
m_NANDTiming.m_u8DataSetup = 80
m_NANDTiming.m_u8DataHold = 60
m_NANDTiming.m_u8AddressSetup = 25
m_NANDTiming.m_u8DSAMPLE_TIME = 6
m_u32PageDataSize = 4096
m_u32TotalPageSize = 4224
m_u32SectorsPerBlock = 64
m_u32NumberOfNANDs = 0
m_u32TotalInternalDie = 0
m_u32CellType = 0
m_u32EccBlockNEccType = 4
m_u32EccBlock0Size = 512
m_u32EccBlockNSize = 512
m_u32EccBlock0EccType = 4
m_u32MetadataBytes = 10
m_u32NumEccBlocksPerPage = 7
m_u32EccBlockNEccLevelSDK = 0
m_u32EccBlock0SizeSDK = 0
m_u32EccBlockNSizeSDK = 0
m_u32EccBlock0EccLevelSDK = 0
m_u32NumEccBlocksPerPageSDK = 0
m_u32MetadataBytesSDK = 0
m_u32EraseThreshold = 0
m_u32Firmware1_startingPage = 512
m_u32Firmware2_startingPage = 131328
m_u32PagesInFirmware1 = 53
m_u32PagesInFirmware2 = 53
m_u32DBBTSearchAreaStartAddress = 256
m_u32BadBlockMarkerByte = 3995
m_u32BadBlockMarkerStartBit = 0
m_u32BBMarkerPhysicalOffset = 4096
m_u32BCHType = 0
m_NANDTMTiming.m_u32TMTiming2_ReadLatency = 0
m_NANDTMTiming.m_u32TMTiming2_PreambleDelay = 0
m_NANDTMTiming.m_u32TMTiming2_CEDelay = 0
m_NANDTMTiming.m_u32TMTiming2_PostambleDelay = 0
m_NANDTMTiming.m_u32TMTiming2_CmdAddPause = 0
m_NANDTMTiming.m_u32TMTiming2_DataPause = 0
m_NANDTMTiming.m_u32TMSpeed = 0
m_NANDTMTiming.m_u32TMTiming1_BusyTimeout = 0
m_u32DISBBM = 0
DBBT
m_u32Checksum = 0x00000000
m_u32FingerPrint = 0x54424244
m_u32Version = 0x01000000
m_u32DBBTNumOfPages = 1
BBTN#0
uNAND = 0
uNumberBB = 11
BADBLOCKS:
0x45 0xac 0x18e 0x600 0x601 0x6e8 0x987 0x989 0xe00 0xe01 0xe96
Firmware: image #0 @ 0x200000 size 0x35000 - available 0x1ff00000
Firmware: image #1 @ 0x20100000 size 0x35000 - available 0x1ff00000
-------------- Start to write the [ FCB ] -----
mtd: erasing @0:0x0-0x40000
mtd: Writing FCB0 [ @0:0x0 ] (1080) *
mtd: erasing @0:0x40000-0x80000
mtd: Writing FCB1 [ @0:0x40000 ] (1080) *
mtd: erasing @0:0x80000-0xc0000
mtd: Writing FCB2 [ @0:0x80000 ] (1080) *
mtd: erasing @0:0xc0000-0x100000
mtd: Writing FCB3 [ @0:0xc0000 ] (1080) *
mtd_commit_bcb(FCB): status 0
-------------- Start to write the [ DBBT ] -----
mtd: erasing @0:0x100000-0x140000
mtd: Writing DBBT0 [ @0:0x100000 ] (1000) *
mtd: erasing @0:0x140000-0x180000
mtd: Writing DBBT1 [ @0:0x140000 ] (1000) *
mtd: erasing @0:0x180000-0x1c0000
mtd: Writing DBBT2 [ @0:0x180000 ] (1000) *
mtd: erasing @0:0x1c0000-0x200000
mtd: Writing DBBT3 [ @0:0x1c0000 ] (1000) *
mtd_commit_bcb(DBBT): status 0
mtd: PUTTING down DBBT0 BBTN0 @0x104000 (0x1000)
mtd: PUTTING down DBBT1 BBTN0 @0x144000 (0x1000)
mtd: PUTTING down DBBT2 BBTN0 @0x184000 (0x1000)
mtd: PUTTING down DBBT3 BBTN0 @0x1c4000 (0x1000)
---------- Start to write the [ u-boot.bin ]----
mtd: Writting u-boot.bin: #0 @0: 0x00200000 - 0x00235000
mtd: erasing @0:0x200000-0x240000
mtd: The last page is not full : 1796
mtd: We write one page for save guard. *
mtd: Writting u-boot.bin: #1 @0: 0x20100000 - 0x20135000
mtd: erasing @0:0x20100000-0x20140000
mtd: The last page is not full : 1796
mtd: We write one page for save guard. *
> ./kobs-ng dump -v
MTD CONFIG:
chip_0_device_path = "/dev/mtd0"
chip_1_device_path = "(null)"
search_exponent = 2
data_setup_time = 80
data_hold_time = 60
address_setup_time = 25
data_sample_time = 6
row_address_size = 3
column_address_size = 2
read_command_code1 = 0
read_command_code2 = 48
boot_stream_major_version = 1
boot_stream_minor_version = 0
boot_stream_sub_version = 0
ncb_version = 3
boot_stream_1_address = 0
boot_stream_2_address = 0
mtd: opening: "/dev/mtd0"
mtd: '/dev/mtd0' bad block @ 0x1140000 (MTD)
mtd: '/dev/mtd0' bad block @ 0x2b00000 (MTD)
mtd: '/dev/mtd0' bad block @ 0x6380000 (MTD)
mtd: '/dev/mtd0' bad block @ 0x18000000 (MTD)
mtd: '/dev/mtd0' bad block @ 0x18040000 (MTD)
mtd: '/dev/mtd0' bad block @ 0x1ba00000 (MTD)
mtd: '/dev/mtd0' bad block @ 0x261c0000 (MTD)
mtd: '/dev/mtd0' bad block @ 0x26240000 (MTD)
mtd: '/dev/mtd0' bad block @ 0x38000000 (MTD)
mtd: '/dev/mtd0' bad block @ 0x38040000 (MTD)
mtd: '/dev/mtd0' bad block @ 0x3a580000 (MTD)
NFC geometry :
ECC Strength : 8
Page Size in Bytes : 4224
Metadata size : 10
ECC Chunk Size in byte : 512
ECC Chunk count : 8
Block Mark Byte Offset : 3995
Block Mark Bit Offset : 0
====================================================
mtd: opened '/dev/mtd0' - '(null)'
mtd: partition #0
type = 4
flags = 17408
size = 1073741824
erasesize = 262144
writesize = 4096
oobsize = 128
blocks = 4096
BAD: 0x1140000 0x2b00000 0x6380000 0x18000000 0x18040000 0x1ba00000 0x261c0000 0x26240000 0x38000000 0x38040000 0x3a580000
mtd: fingerprints mismatch @0:0x0
mtd: fingerprints mismatch @0:0x40000
mtd: fingerprints mismatch @0:0x80000
mtd: fingerprints mismatch @0:0xc0000
mtd: NCB0 not found
mtd: fingerprints mismatch @0:0x100000
mtd: fingerprints mismatch @0:0x140000
mtd: fingerprints mismatch @0:0x180000
mtd: fingerprints mismatch @0:0x1c0000
mtd: NCB1 not found
mtd: neither NCB1 or NCB2 found ERROR
Unable to load boot structures
>>>>
Ma I know is there something wrong with my flash? Thanks!
For clarification, is version 1.3 needed for the dump command on i.MX6 or is 1.3 needed for i.MX6 period? Also, I would also like the source code for version 1.3 if possible. Thanks.
The source code of kobs-ng version 1.3 is now available in Linux BSP release L3.0.35_4.1.0_130816. After installing the LTIB, type command "litb -m prep -p kobs-ng" to get the source code.
The kobs-ng utility helps to program the u-boot to the NAND flash. It is usually run in the manufacturing tool and you can refer to the ucl2.xml in update profile in manufacturing tool for an example.
Both BSP and manufacturing tool can be downloaded at www.freescale.com.
How To Find LTIB L3.0.35_4.1.0_130816 with kobs-ng source code
The Freescale website does an excellent job of obfuscating this information. However, I found it by:
After clicking through the license agreement, the LTIB L3.0.35_4.1.0_130816 download starts.
The direct link is in this post: i.MX 6 Q/D L3.0.35_1.1.0 GA release
Too bad the Freescale people on this site couldn't provide this information as a basic courtesy to their user commuity.
Best regards,
- yba