Hi.
I wonder if some one knows if it's possible to add NAT in the iptables (Yocto project)?
I checked in the .config file, but there seems to be no flag for that.
Is this something that is planned to be included?
Thanks,
Niklas
已解决! 转到解答。
I managed to figure it out.
First I had to enable Netfilter connection tracking support in the Core Netfilter Configuration menu.
After that I go to IP: Netfilter Configuration menu, and enable IPv4 connection tracking support.
Well run
$ make ARCH=arm CROSS_COMPILE=... menuconfig
Then navigate into Networking support -> Networking options -> Network packet filtering framework (Netfilter) -> IP: Netfilter Configuration -> IP tables support (required for filtering/masq/NAT)
... or you can just hit the 'slash' [/] key and type "IP_NF_IPTABLES" , which will give you the exact location of the config option.
I managed to figure it out.
First I had to enable Netfilter connection tracking support in the Core Netfilter Configuration menu.
After that I go to IP: Netfilter Configuration menu, and enable IPv4 connection tracking support.
I'm glad to hear that it's possible, but could you share a noob-friendly list of everything that needs to be enabled to get iptables NAT working.
I tried just bitbaking the iptables package and created an iptables.ipk however on installation it warned that I was missing the kernel modules so I figure I might as well rebuild the whole thing since I'll need an image eventually anyway.
I can start the menuconfig and get down to IP tables support (required for filtering/masq/NAT)
But I can't find anywhere to enable NAT, to set the NF_NAT flag (and I can't find the NF_NAT in the .config file either).