imx8qxp 降频

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

imx8qxp 降频

929 Views
myy
Contributor II

你好,我想问一下imx8qxp cpu降频的温度阈值是多少?

谢谢

0 Kudos
Reply
2 Replies

907 Views
BiyongSUN
NXP Employee
NXP Employee

i.MX8QXP has two thermal zones. 

BSP default dts is 

cpu-thermal0:

passive: 107000

critical: 127000

pmic-thermal0:

passive: 110000

critical: 125000

passive is to do protect. such as down rate of the frequency. 

critical will start extremal action such as reboot or hang the cpu.

Suggest you can read the code, if you are a software engineer.

 

at runtime:

cpu-thermal0:

cat /sys/devices/virtual/thermal/thermal_zone0/trip_point_0_temp
cat /sys/devices/virtual/thermal/thermal_zone0/trip_point_1_temp

pmic-thermal0:

cat /sys/devices/virtual/thermal/thermal_zone1/trip_point_0_temp
cat /sys/devices/virtual/thermal/thermal_zone1/trip_point_1_temp

 

This is linux knowledge, not imx. next time check the linux document first.

Suggest you read the document to know more about thermal in Linux.

linux/Documentation/driver-api/thermal/sysfs-api.rst

 

policy
One of the various thermal governors used for a particular zone.

RW, Required

available_policies
Available thermal governors which can be used for a particular zone.

RO, Required

`trip_point_[0-*]_temp`
The temperature above which trip point will be fired.

Unit: millidegree Celsius

RO, Optional

`trip_point_[0-*]_type`
Strings which indicate the type of the trip point.

E.g. it can be one of critical, hot, passive, `active[0-*]` for ACPI
thermal zone.

RO, Optional

`trip_point_[0-*]_hyst`
The hysteresis value for a trip point, represented as an integer
Unit: Celsius
RW, Optional

`cdev[0-*]`

 

0 Kudos
Reply

915 Views
joanxie
NXP TechSupport
NXP TechSupport

refer to the dts file, the threshold temperature is 127

0 Kudos
Reply