Hi All,
I have a problem streaming from imx8mp AP to a simple RTP client.
The example in the i.MX 8 GStreamer User Guide section 10.1.5 is using the parameter sprop-parameter-sets as a key for the server and the client. This is working fine when I am streaming to VLC client. The problem is that the client, I need to connect too, does not have the provision to use the sprop-parameter-sets parameter.
The original server coomnad line is
gst-launch-1.0 -v filesrc location=FileName.mov ! qtdemux ! rtph264pay ! udpsink host=Client_IP port=5004
How can I modify this command to stream without the sprop-parameter-sets parameter?
Thank you
Hello,
I think the following Community document would be of help on what you're trying to achieve:
https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/Audio-Video-trough-Camera-stream-and-gst...
Best regards,
Aldo.