imx6ulevk nand烧写

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

imx6ulevk nand烧写

3,079件の閲覧回数
xinjianlu
Contributor II

在原理图上QSPI芯片去掉,换成NAND FLASH K9F2G08U0A

用L4.1.15_2.0.0-ga_mfg-tools\L4.1.15_2.0.0-ga_mfg-tools\mfgtools-with-rootfs\mfgtools-with-rootfs\mfgtools下

mfgtool2-yocto-mx-evk-nand.vbs烧-写 出现如下的问题,烧写失败

Advanced Linux Sound Architecture Driver Initialized.
Switched to clocksource mxc_timer1
NET: Registered protocol family 2
TCP established hash table entries: 4096 (order: 2, 16384 bytes)
TCP bind hash table entries: 4096 (order: 3, 32768 bytes)
TCP: Hash tables configured (established 4096 bind 4096)
UDP hash table entries: 256 (order: 1, 8192 bytes)
UDP-Lite hash table entries: 256 (order: 1, 8192 bytes)
NET: Registered protocol family 1
RPC: Registered named UNIX socket transport module.
RPC: Registered udp transport module.
RPC: Registered tcp transport module.
RPC: Registered tcp NFSv4.1 backchannel transport module.
Trying to unpack rootfs image as initramfs...
Freeing initrd memory: 8392K (83800000 - 84032000)
imx rpmsg driver is registered.
Bus freq driver module loaded
futex hash table entries: 256 (order: 2, 16384 bytes)
VFS: Disk quotas dquot_6.6.0
VFS: Dquot-cache hash table entries: 1024 (order 0, 4096 bytes)
NFS: Registering the id_resolver key type
Key type id_resolver registered
Key type id_legacy registered
jffs2: version 2.2. (NAND) ? 2001-2006 Red Hat, Inc.
fuse init (API version 7.23)
io scheduler noop registered
io scheduler deadline registered
io scheduler cfq registered (default)
imx-weim 21b8000.weim: Driver registered.
backlight supply power not found, using dummy regulator
21c8000.lcdif supply lcd not found, using dummy regulator
mxsfb 21c8000.lcdif: failed to find mxc display driver
Console: switching to colour frame buffer device 60x34
mxsfb 21c8000.lcdif: initialized
imx-sdma 20ec000.sdma: no event needs to be remapped
imx-sdma 20ec000.sdma: loaded firmware 3.3
imx-sdma 20ec000.sdma: initialized
2020000.serial: ttymxc0 at MMIO 0x2020000 (irq = 20, base_baud = 5000000) is a IMX
console [ttymxc0] enabled
21e8000.serial: ttymxc1 at MMIO 0x21e8000 (irq = 234, base_baud = 5000000) is a IMX
imx sema4 driver is registered.
[drm] Initialized drm 1.1.0 20060810
[drm] Initialized vivante 1.0.0 20120216 on minor 0
brd: module loaded
loop: module loaded
nand: device found, Manufacturer ID: 0xec, Chip ID: 0xda
nand: Samsung NAND 256MiB 3,3V 8-bit
nand: 256 MiB, SLC, erase size: 128 KiB, page size: 2048, OOB size: 64
gpmi-nand 1806000.gpmi-nand: use legacy bch geometry
Bad block table found at page 131008, version 0x01
Bad block table found at page 130944, version 0x01
nand_read_bbt: bad block at 0x0000068a0000
nand_read_bbt: bad block at 0x00000e1e0000
gpmi-nand 1806000.gpmi-nand: driver registered.
20b4000.ethernet supply phy not found, using dummy regulator
pps pps0: new PPS source ptp0
libphy: fec_enet_mii_bus: probed
fec 20b4000.ethernet eth0: registered PHC device 0
2188000.ethernet supply phy not found, using dummy regulator
pps pps1: new PPS source ptp1
fec 2188000.ethernet eth1: registered PHC device 1
ehci_hcd: USB 2.0 'Enhanced' Host Controller (EHCI) Driver
ehci-mxc: Freescale On-Chip EHCI Host driver
usbcore: registered new interface driver usb-storage
2184800.usbmisc supply vbus-wakeup not found, using dummy regulator
2184000.usb supply vbus not found, using dummy regulator
2184200.usb supply vbus not found, using dummy regulator
ci_hdrc ci_hdrc.1: EHCI Host Controller
ci_hdrc ci_hdrc.1: new USB bus registered, assigned bus number 1
ci_hdrc ci_hdrc.1: USB 2.0 started, EHCI 1.00
hub 1-0:1.0: USB hub found
hub 1-0:1.0: 1 port detected
Mass Storage Function, version: 2009/09/11
LUN: removable file: (no medium)
LUN: removable read only file: /fat
Number of LUNs=1
Number of LUNs=1
g_mass_storage gadget: Mass Storage Gadget, version: 2009/09/11
g_mass_storage gadget: g_mass_storage ready
mousedev: PS/2 mouse device common for all mice
input: 20cc000.snvs:snvs-powerkey as /devices/platform/soc/2000000.aips-bus/20cc000.snvs/20cc000.snvs:snvs-powerkey/input/input0
input: iMX6UL TouchScreen Controller as /devices/platform/soc/2000000.aips-bus/2040000.tsc/input/input1
snvs_rtc 20cc000.snvs:snvs-rtc-lp: rtc core: registered 20cc000.snvs:snvs-r as rtc0
i2c /dev entries driver
IR NEC protocol handler initialized
IR RC5(x/sz) protocol handler initialized
IR RC6 protocol handler initialized
IR JVC protocol handler initialized
IR Sony protocol handler initialized
IR SANYO protocol handler initialized
IR Sharp protocol handler initialized
IR MCE Keyboard/mouse protocol handler initialized
IR XMP protocol handler initialized
pxp-v4l2 pxp_v4l2: initialized
imx2-wdt 20bc000.wdog: use WDOG_B to reboot.
imx2-wdt 20bc000.wdog: timeout 60 sec (nowayout=0)
sdhci: Secure Digital Host Controller Interface driver
sdhci: Copyright(c) Pierre Ossman
sdhci-pltfm: SDHCI platform and OF driver helper
/soc/aips-bus@02100000/usdhc@02190000: voltage-ranges unspecified
sdhci-esdhc-imx 2190000.usdhc: Got CD GPIO
sdhci-esdhc-imx 2190000.usdhc: No vqmmc regulator found
mmc0: SDHCI controller on 2190000.usdhc [2190000.usdhc] using ADMA
usbcore: registered new interface driver usbhid
usbhid: USB HID core driver
NET: Registered protocol family 10
sit: IPv6 over IPv4 tunneling driver
NET: Registered protocol family 17
Key type dns_resolver registered
Registering SWP/SWPB emulation handler
snvs_rtc 20cc000.snvs:snvs-rtc-lp: setting system clock to 1970-01-01 00:32:29 UTC (1949)
VSD_3V3: disabling
can-3v3: disabling
clk: Not disabling unused clocks
ALSA device list:
  No soundcards found.
Freeing unused kernel memory: 384K (80922000 - 80982000)
g_mass_storage gadget: high-speed config #1: Linux File-Backed Storage
Starting UTP
uuc 0.5 [built Sep 16 2016 02:36:28]
UTP: Waiting for device to appear
UTP: file/device node /dev/utp already exists
cpu_id is 0
UTP: received command '$ mount -t debugfs debugfs /sys/kernel/debug'
UTP: executing "mount -t debugfs debugfs /sys/kernel/debug"
UTP: sending Success to kernel for command $ mount -t debugfs debugfs /sys/kernel/debug.
utp_poll: pass returned.
UTP: received command '$ flash_erase /dev/mtd0 0 0'
UTP: executing "flash_erase /dev/mtd0 0 0"
Erasing 128 Kibyte @ 6880000 -- 40 % complete flash_erase: Skipping bad block at 068a0000
Erasing 128 Kibrandom: nonblocking pool is initialized
Erasing 128 Kibyte @ e1c0000 -- 88 % complete flash_erase: Skipping bad block at 0e1e0000
Erasing 128 Kibyte @ fc60000 -- 98 %utp_poll: pass returned.
Erasing 128 Kibyte @ ff60000 -- 99 % complete flash_erase: Skipping bad block at 0ff80000
flash_erase: Skipping bad block at 0ffa0000
flash_erase: Skipping bad block at 0ffc0000
flash_erase: Skipping bad block at 0ffe0000
Erasing 128 Kibyte @ ffe0000 -- 100 % complete
UTP: sending Success to kernel for command $ flash_erase /dev/mtd0 0 0.
UTP: received command 'send'
UTP: sending Success to kernel for command send.
UTP: received command '$ kobs-ng init -x -v --chip_0_device_path=/dev/mtd0 $FILE'
UTP: executing "kobs-ng init -x -v --chip_0_device_path=/dev/mtd0 $FILE"
MTD CONFIG:
  chip_0_device_path = "/dev/mtd0"
  chip_1_device_path = "(null)"
  search_exponent = 2
  data_setup_time = 80
  data_hold_time = 60
  address_setup_time = 25
  data_sample_time = 6
  row_address_size = 3
  column_address_size = 2
  read_command_code1 = 0
  read_command_code2 = 48
  boot_stream_major_version = 1
  boot_stream_minor_version = 0
  boot_stream_sub_version = 0
  ncb_version = 3
  boot_stream_1_address = 0
  boot_stream_2_address = 0
         -- We add the 1k-padding to the uboot.
.tmp_kobs_ng: verifying using key '00000000000000000000000000000000'
.tmp_kobs_ng: is a valid bootstream for key '00000000000000000000000000000000'
mtd: use new bch layout raw access mode
mtd: opening: "/dev/mtd0"
mtd: '/dev/mtd0' bad block @ 0x68a0000 (MTD)
mtd: '/dev/mtd0' bad block @ 0xe1e0000 (MTD)
mtd: '/dev/mtd0' bad block @ 0xff80000 (MTD)
mtd: '/dev/mtd0' bad block @ 0xffa0000 (MTD)
mtd: '/dev/mtd0' bad block @ 0xffc0000 (MTD)
mtd: '/dev/mtd0' bad block @ 0xffe0000 (MTD)
NFC geometry :
        ECC Strength       : 8
        Page Size in Bytes : 2112
        Metadata size      : 10
        ECC Chunk Size in byte : 512
        ECC Chunk count        : 4
        Block Mark Byte Offset : 1999
        Block Mark Bit Offset  : 0
====================================================
mtd: opened '/dev/mtd0' - '(null)'
mtd: max_boot_stream_size_in_bytes = 133693440
mtd: boot_stream_size_in_bytes = 412440
mtd: boot_stream_size_in_pages = 202
mtd: #1 0x00100000 - 0x08080000 (0x00164b18)
mtd: #2 0x08080000 - 0x10000000 (0x080e4b18)
FCB
  m_u32Checksum = 0x00000000
  m_u32FingerPrint = 0x20424346
  m_u32Version = 0x01000000
  m_NANDTiming.m_u8DataSetup = 80
  m_NANDTiming.m_u8DataHold = 60
  m_NANDTiming.m_u8AddressSetup = 25
  m_NANDTiming.m_u8DSAMPLE_TIME = 6
  m_u32PageDataSize = 2048
  m_u32TotalPageSize = 2112
  m_u32SectorsPerBlock = 64
  m_u32NumberOfNANDs = 0
  m_u32TotalInternalDie = 0
  m_u32CellType = 0
  m_u32EccBlockNEccType = 4
  m_u32EccBlock0Size = 512
  m_u32EccBlockNSize = 512
  m_u32EccBlock0EccType = 4
  m_u32MetadataBytes = 10
  m_u32NumEccBlocksPerPage = 3
  m_u32EccBlockNEccLevelSDK = 0
  m_u32EccBlock0SizeSDK = 0
  m_u32EccBlockNSizeSDK = 0
  m_u32EccBlock0EccLevelSDK = 0
  m_u32NumEccBlocksPerPageSDK = 0
  m_u32MetadataBytesSDK = 0
  m_u32EraseThreshold = 0
  m_u32Firmware1_startingPage = 512
  m_u32Firmware2_startingPage = 65792
  m_u32PagesInFirmware1 = 202
  m_u32PagesInFirmware2 = 202
  m_u32DBBTSearchAreaStartAddress = 256
  m_u32BadBlockMarkerByte = 1999
  m_u32BadBlockMarkerStartBit = 0
  m_u32BBMarkerPhysicalOffset = 2048
  m_u32BCHType = 0
  m_NANDTMTiming.m_u32TMTiming2_ReadLatency = 0
  m_NANDTMTiming.m_u32TMTiming2_PreambleDelay = 0
  m_NANDTMTiming.m_u32TMTiming2_CEDelay = 0
  m_NANDTMTiming.m_u32TMTiming2_PostambleDelay = 0
  m_NANDTMTiming.m_u32TMTiming2_CmdAddPause = 0
  m_NANDTMTiming.m_u32TMTiming2_DataPause = 0
  m_NANDTMTiming.m_u32TMSpeed = 0
  m_NANDTMTiming.m_u32TMTiming1_BusyTimeout = 0
  m_u32DISBBM = 0
  m_u32BBMarkerPhysicalOffsetInSpareData = 0
  m_u32OnfiSyncEnable = 0
  m_NANDONFITiming.m_u32ONFISpeed = 0
  m_NANDONFITiming.m_u32ONFITiming_ReadLatency = 0
  m_NANDONFITiming.m_u32ONFITiming_CEDelay = 0
  m_NANDONFITiming.m_u32ONFITiming_PreambleDelay = 0
  m_NANDONFITiming.m_u32ONFITiming_PostambleDelay = 0
  m_NANDONFITiming.m_u32ONFITiming_CmdAddPause = 0
  m_NANDONFITiming.m_u32ONFITiming_DataPause = 0
  m_NANDONFITiming.m_u32ONFITiming_BusyTimeout = 0
  m_u32DISBBSearch = 0
  m_u32RandomizerEnable = 0
  m_u32ReadRetryEnable = 0
  m_u32ReadRetrySeqLength = 0
DBBT
  m_u32Checksum = 0x00000000
  m_u32FingerPrint = 0x54424244
  m_u32Version = 0x01000000
  m_u32DBBTNumOfPages = 1
BBTN#0
  uNAND = 0
  uNumberBB = 6
  BADBLOCKS:
     0x345 0x70f 0x7fc 0x7fd 0x7fe 0x7ff
Firmware: image #0 @ 0x100000 size 0x65000 - available 0x7f80000
Firmware: image #1 @ 0x8080000 size 0x65000 - available 0x7f80000
-------------- Start to write the [ FCB ] -----
mtd: erasing @0:0x0-0x20000
mtd: Writing FCB0 [ @0:0x0 ] (840) *
mtd: erasing @0:0x20000-0x40000
mtd: Writing FCB1 [ @0:0x20000 ] (840) *
mtd: erasing @0:0x40000-0x60000
mtd: Writing FCB2 [ @0:0x40000 ] (840) *
mtd: erasing @0:0x60000-0x80000
mtd: Writing FCB3 [ @0:0x60000 ] (840) *
mtd_commit_bcb(FCB): status 0

-------------- Start to write the [ DBBT ] -----
mtd: erasing @0:0x80000-0xa0000
mtd: Writing DBBT0 [ @0:0x80000 ] (800) *
mtd: erasing @0:0xa0000-0xc0000
mtd: Writing DBBT1 [ @0:0xa0000 ] (800) *
mtd: erasing @0:0xc0000-0xe0000
mtd: Writing DBBT2 [ @0:0xc0000 ] (800) *
mtd: erasing @0:0xe0000-0x100000
mtd: Writing DBBT3 [ @0:0xe0000 ] (800) *
mtd_commit_bcb(DBBT): status 0

mtd: PUTTING down DBBT0 BBTN0 @0x82000 (0x800)
mtd: PUTTING down DBBT1 BBTN0 @0xa2000 (0x800)
mtd: PUTTING down DBBT2 BBTN0 @0xc2000 (0x800)
mtd: PUTTING down DBBT3 BBTN0 @0xe2000 (0x800)
---------- Start to write the [ .tmp_kobs_ng ]----
mtd: Writting .tmp_kobs_ng: #0 @0: 0x00100000 - 0x00165000
mtd: erasing @0:0x100000-0x120000
mtd: erasing @0:0x120000-0x140000
mtd: erasing @0:0x140000-0x160000
mtd: erasing @0:0x160000-0x180000
mtd: The last page is not full : 792
mtd: We write one page for save guard. *
mtd: Writting .tmp_kobs_ng: #1 @0: 0x08080000 - 0x080e5000
mtd: erasing @0:0x8080000-0x80a0000
mtd: erasing @0:0x80a0000-0x80c0000
mtd: erasing @0:0x80c0000-0x80e0000
mtd: erasing @0:0x80e0000-0x8100000
mtd: The last page is not full : 792
mtd: We write one page for save guard. *
UTP: sending Success to kernel for command $ kobs-ng init -x -v --chip_0_device_path=/dev/mtd0 $FILE.
utp_poll: pass returned.
UTP: received command '$ flash_erase /dev/mtd1 0 0'
UTP: executing "flash_erase /dev/mtd1 0 0"
flash_erase: error!: /dev/mtd1
             error 2 (No such file or directory)
UTP: sending Non-success to kernel for command $ flash_erase /dev/mtd1 0 0.
utp_poll: exit with status 65280

请问这问题出在哪里

ラベル(1)
0 件の賞賛
返信
3 返答(返信)

1,512件の閲覧回数
b36401
NXP Employee
NXP Employee

Please doublecheck device enumeration. I mean possibly NAND is not exactly /dev/mtd1

Have a great day,
Victor

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

1,512件の閲覧回数
brunoferrarezi
Contributor II

Hi Victor Linnik,

I have the same problem here im my board. How can I chek the enumeration?

Thank you.

Bruno.

0 件の賞賛
返信

1,512件の閲覧回数
xinjianlu
Contributor II

不太明白,请细一点说明

0 件の賞賛
返信