imx6qsabreauto is not booting?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

imx6qsabreauto is not booting?

942 次查看
madhusudhanredd
Contributor I

Hello all,

Currently, I am working on bring up the imx6qsabreauto board. I connected the UART cable from PC to the board.

I inseted SDcard which contains linux binary image file.

Once after Power On, am unable to see anything on the serial terminal.

Please give me some advises how to bring up this board?

Regards,

Madhu Sudhan Reddy N.

0 项奖励
回复
2 回复数

634 次查看
madhusudhanredd
Contributor I

Hi Dan Wang,

Thanks for your response.

yes, i checked it is in proper boot mode i.e boot from sdcard.

S1 :  0 1 0 0 1 0 0 0 0 0

S2 :  0 0 1 0

S3 :  0 0 1 0

We checked the CPU clock and current all these are fine.

then also it is not booting, I am unable to see anything on my serial terminal.

Regards,

Madhu Sudhan Reddy N.

0 项奖励
回复

634 次查看
Rita_Wang
NXP TechSupport
NXP TechSupport

Hi Madhu Sudhan Reddy N,

Have you set proper boot mode of your board, boot from SD card? Please have a check first.
Have a great day,
Dan

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Mark Correct  button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复