Hello,
Please look at the following
iMX6 PCIe PCIe RC mode imx_pcie_pltfm_probe entering.
Have a great day,
Yuri
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hello,
I am using INTEL pc82573E(pcie to 1000Gbit ethernet) on our custom IMX6Q board based on SabreSD board. but it seems that could not recognise the devcie properly.
the kernel is Linux 3.0.35-imx,and we choose board (mx6q_sabresd) on LTIB config.
here is what i have done:
add a star to:
System Type -> Freescale MXC Implementations -> PCI Express support
Bus support -> Message Signaled Interrupts (MSI and MSI-X)
Bus support -> PCI Express Support
Device Drivers -> Network Device support -> Ethernet (1000 Mbit)
Device Drivers -> Network Device support -> Ethernet (1000 Mbit) -> Realtek 8169 gigabit ethernet support
Device Drivers -> Network Device support -> Ethernet (1000 Mbit) -> Intel(R) PRO/1000 Gigabit Ethernet support
Device Drivers -> Network Device support -> Ethernet (1000 Mbit) -> Intel(R) PRO/1000 PCI-Express Gigabit Ethernet support
Device Drivers -> Network Device support -> Ethernet (1000 Mbit) -> IP1000 Gigabit Ethernet support
Device Drivers -> Network Device support -> Ethernet (1000 Mbit) -> Intel(R) 82575/82576 PCI-Express Gigabit Ethernet support
Device Drivers -> Network Device support -> Ethernet (1000 Mbit) -> Intel(R) 82576 Virtual Function Ethernet support
and remove the star from: make menuconfig -> Device Drivers -> Network Device support -> Ethernet (10 or 100Mb)
after compile the kernel i use MfgTool2 to load the uImage to the emmc on board.
But the question remains.
Hardware should be no problem, because my colleagues successfully before.
so what can i do?
Have a great day,
Pei