imx6q HDMI doesn't work. (We use customized board)

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

imx6q HDMI doesn't work. (We use customized board)

跳至解决方案
964 次查看
leeinchul
Contributor II

Dear all,

We use customized board based on imx6q sabreai board and linux OS. HDMI schematic(pin mux and all passive element) is same with sabreai. But we don't use audio function(hw codec doesn't be applied)

When we use same binary image, sabreai works but customize board doesn't work(but hotplug is detected).

If hw codec doesn't be applied, Doesn't HDMI work?

If we have to imx6zeng modify kernel source, would give me the check point?

Thanks and best regard.

1 解答
782 次查看
leeinchul
Contributor II

Hi, Saurabh.

We solved this issue.

We missed HW(CM2020) check point.

TMDS lines must be connected in PCB.

제목 없음.png

Thanks and best regards.

在原帖中查看解决方案

2 回复数
782 次查看
saurabh206
Senior Contributor III

Hi,

Lee

HDMI display work without Audio also.

Which BSP you are using with your hardware?

Thanks

Saurabh

783 次查看
leeinchul
Contributor II

Hi, Saurabh.

We solved this issue.

We missed HW(CM2020) check point.

TMDS lines must be connected in PCB.

제목 없음.png

Thanks and best regards.