imx6q HDMI doesn't work. (We use customized board)

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

imx6q HDMI doesn't work. (We use customized board)

ソリューションへジャンプ
963件の閲覧回数
leeinchul
Contributor II

Dear all,

We use customized board based on imx6q sabreai board and linux OS. HDMI schematic(pin mux and all passive element) is same with sabreai. But we don't use audio function(hw codec doesn't be applied)

When we use same binary image, sabreai works but customize board doesn't work(but hotplug is detected).

If hw codec doesn't be applied, Doesn't HDMI work?

If we have to imx6zeng modify kernel source, would give me the check point?

Thanks and best regard.

1 解決策
781件の閲覧回数
leeinchul
Contributor II

Hi, Saurabh.

We solved this issue.

We missed HW(CM2020) check point.

TMDS lines must be connected in PCB.

제목 없음.png

Thanks and best regards.

元の投稿で解決策を見る

2 返答(返信)
781件の閲覧回数
saurabh206
Senior Contributor III

Hi,

Lee

HDMI display work without Audio also.

Which BSP you are using with your hardware?

Thanks

Saurabh

782件の閲覧回数
leeinchul
Contributor II

Hi, Saurabh.

We solved this issue.

We missed HW(CM2020) check point.

TMDS lines must be connected in PCB.

제목 없음.png

Thanks and best regards.