imx6q HDMI doesn't work. (We use customized board)

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

imx6q HDMI doesn't work. (We use customized board)

Jump to solution
747 Views
leeinchul
Contributor II

Dear all,

We use customized board based on imx6q sabreai board and linux OS. HDMI schematic(pin mux and all passive element) is same with sabreai. But we don't use audio function(hw codec doesn't be applied)

When we use same binary image, sabreai works but customize board doesn't work(but hotplug is detected).

If hw codec doesn't be applied, Doesn't HDMI work?

If we have to imx6zeng modify kernel source, would give me the check point?

Thanks and best regard.

1 Solution
565 Views
leeinchul
Contributor II

Hi, Saurabh.

We solved this issue.

We missed HW(CM2020) check point.

TMDS lines must be connected in PCB.

제목 없음.png

Thanks and best regards.

View solution in original post

2 Replies
565 Views
saurabh206
Senior Contributor III

Hi,

Lee

HDMI display work without Audio also.

Which BSP you are using with your hardware?

Thanks

Saurabh

566 Views
leeinchul
Contributor II

Hi, Saurabh.

We solved this issue.

We missed HW(CM2020) check point.

TMDS lines must be connected in PCB.

제목 없음.png

Thanks and best regards.