imx6 uboot can`t ping itself or pc success

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

imx6 uboot can`t ping itself or pc success

1,316 Views
teillee
Contributor I

Now ,our board`s NET part is done refer to imx6_sabreltie ,but we can`t ping it and pc successful, when we intend to use "TFTP"  to download the uImage .I want to know why and how could we solve the problem. Here are my schematics, and the board application is attached:

19058_19058.pngQQ截图20150123140212.png19060_19060.pngETH_MD...png19059_19059.pngQQ截图20150121112141.png19051_19051.pngQQ截图20150121112310.png

Original Attachment has been moved to: mx6q_sabrelite.c.zip

Labels (1)
Tags (1)
0 Kudos
Reply
4 Replies

822 Views
alejandrolozan1
NXP Employee
NXP Employee

Hi,

Are you not getting any kind of error when trying to configure the phy?

I noticed that in most of our boards the MDIO signal has a pull up resistor, yours do not. I wonder if you have tried a loopback test between the MPU and the PHY just to check  that the connection between the iMX6 and the PHY is corret.

The Freescal SDK can help you with that.

https://www.freescale.com/webapp/Download?colCode=i.MX6_PLATFORM_SDK&location=null&WT_TYPE=Software%...

Regards,

Alejandro

0 Kudos
Reply

822 Views
teillee
Contributor I

Hi,

Thanks for the reply.I am not getting any kind of error when trying to configure the phy. our board have a 4.7k(R66) pull up resistor on the MDIO signal . there is no problem when i conduct stress tests. but the link led and signal led do not light when I enter uboot commd line and insert cable .why?

0 Kudos
Reply

822 Views
alejandrolozan1
NXP Employee
NXP Employee

The LEDs turn on when the link is up. Have you checked the internal status of the Phy via MDIO as previously suggested?

Alejandro

0 Kudos
Reply

822 Views
saurabh206
Senior Contributor III

Hi,

Send your post to imx community (e.g. i.MX Community ) to get it visible for active members.

Saurabh

0 Kudos
Reply