Hi,
After reviewing the information in
https://freescale.jiveon.com/docs/DOC-105652
https://freescale.jiveon.com/docs/DOC-346065
We still would like to know how to run memory calibration for mass production purposes.
It seems the the the UI version cannot be executed in "batch mode" generating calibration parameters after each cycle. The two other option described in https://freescale.jiveon.com/docs/DOC-105652 are used fro memory stress test and not generation of calibration parameters.
Is there a way to generate calibration parameters in a non-interactive mode? We would like to run the calibration on a large sample of our product.
Thanks,
Yair
解決済! 解決策の投稿を見る。
@yairh
Hello,
Generally section 7.3 (Timing Calibrations Usage) of AN4467 (i.MX 6 Series DDR Calibration)
describes possible calibration policies.
https://www.nxp.com/docs/en/application-note/AN4467.pdf
Usually it is enough to calibrate manually several boards from a batch under different
operation conditions and use average / median values for all boards.
We do not have special calibration tool as You need.
Regards,
Yuri.