imx6 mass production memory calibration

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

imx6 mass production memory calibration

跳至解决方案
1,399 次查看
yairh
Contributor III

Hi, 

After reviewing  the information in

https://freescale.jiveon.com/docs/DOC-105652

https://freescale.jiveon.com/docs/DOC-346065 

We still would like to know how to run memory calibration for mass production purposes. 

It seems the the the UI version cannot be executed in "batch mode" generating calibration parameters after each cycle. The two other option described in https://freescale.jiveon.com/docs/DOC-105652 are used fro memory stress test and not generation of calibration parameters. 

Is there a way to generate calibration parameters in a non-interactive mode? We would like to run the calibration on a large sample of our product. 

 

Thanks,

Yair 

0 项奖励
回复
1 解答
1,381 次查看
yairh
Contributor III

@Yuri 

Thanks for the information. Will review the application note. 

 

Yar

在原帖中查看解决方案

0 项奖励
回复
2 回复数
1,386 次查看
Yuri
NXP Employee
NXP Employee

@yairh 
Hello,

   Generally section 7.3 (Timing Calibrations Usage) of AN4467 (i.MX 6 Series DDR Calibration)
describes possible calibration policies.

https://www.nxp.com/docs/en/application-note/AN4467.pdf

  Usually it is enough to calibrate manually several boards from a batch under different
operation conditions and use average / median values for all boards.

  We do not have special calibration tool as You need.

Regards,
Yuri.

0 项奖励
回复
1,382 次查看
yairh
Contributor III

@Yuri 

Thanks for the information. Will review the application note. 

 

Yar

0 项奖励
回复