imx6 android6.0.1 usb camera

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

imx6 android6.0.1 usb camera

1,670 Views
rudolphhsueh
Contributor III

Hi All,

     I use USB camera on imx6dl.  I cannot use 5M pixel to take picture but 2M pixel is OK. do you have any suggestion?
Thanks.

logcat says:
01-01 00:38:39.994 208 1412 E BufferQueueConsumer: [GraphicBufferSource] releaseBuffer: attempted to release buffer slot 2 but its state was 0
01-01 00:38:40.263 208 1412 E BufferQueueConsumer: [GraphicBufferSource] releaseBuffer: attempted to release buffer slot 3 but its state was 0
01-01 00:38:40.327 208 1412 E BufferQueueConsumer: [GraphicBufferSource] releaseBuffer: attempted to release buffer slot 4 but its state was 0
01-01 00:38:40.425 208 1412 E BufferQueueConsumer: [GraphicBufferSource] releaseBuffer: attempted to release buffer slot 2 but its state was 0
01-01 00:38:40.560 208 1412 E BufferQueueConsumer: [GraphicBufferSource] releaseBuffer: attempted to release buffer slot 1 but its state was 0
01-01 00:38:40.663 208 1412 E BufferQueueConsumer: [GraphicBufferSource] releaseBuffer: attempted to release buffer slot 3 but its state was 0
01-01 00:38:40.784 1332 1332 I CAM_CaptureModule: rudolph add takePictureNow.
01-01 00:38:40.791 1332 1332 I CAM_FilmstripView: [ViewItem:0] mData.renderThumbnail()
01-01 00:38:40.792 1332 1929 V CameraCaptureSession: Session 0: captureBurst - requests [android.hardware.camera2.CaptureRequest@5e4fd072], callback com.android.camera.one.v2.camera2proxy.AndroidCameraCaptureSessionProxy$AndroidCaptureCallback@6b80ada handler Handler (android.os.Handler) {1e0832a}
01-01 00:38:40.850 1332 1924 W LegacyRequestMapper: convertRequestMetadata - control.awbRegions setting is not supported, ignoring value
01-01 00:38:40.850 1332 1924 W LegacyRequestMapper: Only received metering rectangles with weight 0.
01-01 00:38:40.851 1332 1924 W LegacyRequestMapper: mapAeAndFlashMode - Ignore control.aeMode == ON_AUTO_FLASH;camera does not support it
01-01 00:38:40.851 1332 1924 W LegacyMetadataMapper: convertAfModeToLegacy - ignoring unsupported mode 4, defaulting to fixed
01-01 00:38:40.851 1332 1924 W LegacyRequestMapper: convertRequestToMetadata - Ignoring android.lens.focusDistance false, only 0.0f is supported
01-01 00:38:40.911 208 1918 I FslCameraHAL: const camera_metadata_t* Camera::constructDefaultRequestSettings(int32_t):0: type=2
01-01 00:38:41.050 208 252 I FslCameraHAL: ae precature trigger
01-01 00:38:41.206 208 1915 I FslCameraHAL: int32_t VideoStream::configure(android::sp<Stream>): w:800, h:600, sensor format:0x14, stream format:0x103, fps:30, num:3
01-01 00:38:41.208 208 1412 E BufferQueueConsumer: [GraphicBufferSource] releaseBuffer: attempted to release buffer slot 1 but its state was 0
01-01 00:38:41.213 208 252 I FslCameraHAL: virtual int32_t UvcDevice::UvcStream::onDeviceStopLocked()
01-01 00:38:41.240 208 252 I FslCameraHAL: virtual int32_t DMAStream::freeBuffersLocked()
01-01 00:38:41.240 208 252 I FslCameraHAL: freeBufferToIon buffer num:3
01-01 00:38:41.241 208 252 I FslCameraHAL: virtual int32_t UvcDevice::UvcStream::onDeviceConfigureLocked()
01-01 00:38:41.241 208 252 I FslCameraHAL: virtual int32_t DMAStream::onDeviceConfigureLocked()
01-01 00:38:41.241 208 252 I FslCameraHAL: virtual int32_t USPStream::onDeviceConfigureLocked()
01-01 00:38:41.241 208 252 I FslCameraHAL: virtual int32_t MMAPStream::onDeviceConfigureLocked()
01-01 00:38:41.241 208 252 I FslCameraHAL: Width * Height 2592 x 1944 format YUYV, fps: 15
01-01 00:38:41.253 208 252 I FslCameraHAL: virtual int32_t DMAStream::allocateBuffersLocked()
01-01 00:38:41.253 208 252 I FslCameraHAL: allocateBufferFromIon buffer num:2
01-01 00:38:41.339 208 252 I FslCameraHAL: phyalloc ptr:0xa8122000, phy:0x2ff00000, ionSize:10121216
01-01 00:38:41.400 208 252 I FslCameraHAL: phyalloc ptr:0xa6a0a000, phy:0x30900000, ionSize:10121216
01-01 00:38:41.400 208 252 I FslCameraHAL: virtual int32_t UvcDevice::UvcStream::onDeviceStartLocked()
01-01 00:38:41.401 208 252 I FslCameraHAL: buf[0] length:10077696
01-01 00:38:41.401 208 252 I FslCameraHAL: buf[1] length:10077696
01-01 00:38:41.438 1332 1332 W AudioTrack: AUDIO_OUTPUT_FLAG_FAST denied by client; transfer 4, track 48000 Hz, output 44100 Hz
01-01 00:38:41.443 208 431 W audio_hw_primary: out_set_parameters routing=2, ret 0, out -1243028160
01-01 00:38:41.454 208 430 W audio_hw_primary: ret -32, pcm write 768 error wait error: hw 0x40980 app 0x40f80 avail 0x0
01-01 00:38:41.454 208 430 W audio_hw_primary: : Unknown error -32
01-01 00:38:44.878 208 431 W audio_hw_primary: no standby
01-01 00:38:44.951 1332 1924 E RequestThread-0: Hit timeout for jpeg callback!
01-01 00:38:44.951 1332 1924 W CaptureCollector: Jpeg buffers dropped for request: 1
01-01 00:38:44.952 1332 1907 E CameraDevice-JV-0: Lost output buffer reported for frame 83
01-01 00:38:44.965 1332 1924 W LegacyRequestMapper: convertRequestMetadata - control.awbRegions setting is not supported, ignoring value
01-01 00:38:44.965 1332 1924 W LegacyRequestMapper: Only received metering rectangles with weight 0.
01-01 00:38:44.966 1332 1924 W LegacyRequestMapper: mapAeAndFlashMode - Ignore control.aeMode == ON_AUTO_FLASH;camera does not support it
01-01 00:38:44.966 1332 1924 W LegacyMetadataMapper: convertAfModeToLegacy - ignoring unsupported mode 4, defaulting to fixed
01-01 00:38:44.967 1332 1924 W LegacyRequestMapper: convertRequestToMetadata - Ignoring android.lens.focusDistance false, only 0.0f is supported
01-01 00:38:44.979 208 437 E Camera2Client: startPreviewL: Can't start preview in state STILL_CAPTURE
01-01 00:38:44.981 1332 1924 E RequestThread-0: Received device exception during capture call:
01-01 00:38:44.981 1332 1924 E RequestThread-0: java.lang.RuntimeException: startPreview failed
01-01 00:38:44.981 1332 1924 E RequestThread-0: at android.hardware.Camera.startPreview(Native Method)
01-01 00:38:44.981 1332 1924 E RequestThread-0: at android.hardware.camera2.legacy.RequestThreadManager.startPreview(RequestThreadManager.java:288)
01-01 00:38:44.981 1332 1924 E RequestThread-0: at android.hardware.camera2.legacy.RequestThreadManager.doPreviewCapture(RequestThreadManager.java:330)
01-01 00:38:44.981 1332 1924 E RequestThread-0: at android.hardware.camera2.legacy.RequestThreadManager.-wrap3(RequestThreadManager.java)
01-01 00:38:44.981 1332 1924 E RequestThread-0: at android.hardware.camera2.legacy.RequestThreadManager$5.handleMessage(RequestThreadManager.java:802)
01-01 00:38:44.981 1332 1924 E RequestThread-0: at android.os.Handler.dispatchMessage(Handler.java:98)
01-01 00:38:44.981 1332 1924 E RequestThread-0: at android.os.Looper.loop(Looper.java:148)
01-01 00:38:44.981 1332 1924 E RequestThread-0: at android.os.HandlerThread.run(HandlerThread.java:61)
01-01 00:38:44.981 1332 1924 I CameraDeviceState: Legacy camera service transitioning to state ERROR
01-01 00:38:44.985 208 825 E Camera2Client: startPreviewL: Can't start preview in state STILL_CAPTURE
01-01 00:38:44.987 1332 1924 E RequestThread-0: Received device exception during capture call:
01-01 00:38:44.987 1332 1924 E RequestThread-0: java.lang.RuntimeException: startPreview failed
01-01 00:38:44.987 1332 1924 E RequestThread-0: at android.hardware.Camera.startPreview(Native Method)
01-01 00:38:44.987 1332 1924 E RequestThread-0: at android.hardware.camera2.legacy.RequestThreadManager.startPreview(RequestThreadManager.java:288)
01-01 00:38:44.987 1332 1924 E RequestThread-0: at android.hardware.camera2.legacy.RequestThreadManager.doPreviewCapture(RequestThreadManager.java:330)
01-01 00:38:44.987 1332 1924 E RequestThread-0: at android.hardware.camera2.legacy.RequestThreadManager.-wrap3(RequestThreadManager.java)
01-01 00:38:44.987 1332 1924 E RequestThread-0: at android.hardware.camera2.legacy.RequestThreadManager$5.handleMessage(RequestThreadManager.java:802)
01-01 00:38:44.987 1332 1924 E RequestThread-0: at android.os.Handler.dispatchMessage(Handler.java:98)
01-01 00:38:44.987 1332 1924 E RequestThread-0: at android.os.Looper.loop(Looper.java:148)
01-01 00:38:44.987 1332 1924 E RequestThread-0: at android.os.HandlerThread.run(HandlerThread.java:61)
01-01 00:38:44.993 1332 1794 E CAM_FatalErrorHandler: Handling Camera Access Failure:
01-01 00:38:44.993 1332 1794 E CAM_FatalErrorHandler: java.lang.Exception
01-01 00:38:44.993 1332 1794 E CAM_FatalErrorHandler: at com.android.camera.FatalErrorHandlerImpl.onGenericCameraAccessFailure(FatalErrorHandlerImpl.java:84)
01-01 00:38:44.993 1332 1794 E CAM_FatalErrorHandler: at com.android.camera.one.v2.Camera2OneCameraOpenerImpl$1.onError(Camera2OneCameraOpenerImpl.java:154)
01-01 00:38:44.993 1332 1794 E CAM_FatalErrorHandler: at android.hardware.camera2.impl.CameraDeviceImpl$CameraDeviceCallbacks$1.run(CameraDeviceImpl.java:1697)
01-01 00:38:44.993 1332 1794 E CAM_FatalErrorHandler: at android.os.Handler.handleCallback(Handler.java:739)
01-01 00:38:44.993 1332 1794 E CAM_FatalErrorHandler: at android.os.Handler.dispatchMessage(Handler.java:95)
01-01 00:38:44.993 1332 1794 E CAM_FatalErrorHandler: at android.os.Looper.loop(Looper.java:148)
01-01 00:38:44.993 1332 1794 E CAM_FatalErrorHandler: at android.os.HandlerThread.run(HandlerThread.java:61)
01-01 00:38:44.993 1332 1794 E CAM_CameraUtil: Show fatal error dialog
01-01 00:38:45.078 197 509 E BufferQueueProducer: [com.android.camera2/com.android.camera.CameraLauncher] dequeueBuffer: can't dequeue multiple buffers without setting the buffer count
01-01 00:38:46.898 208 1412 E BufferQueueConsumer: [GraphicBufferSource] releaseBuffer: attempted to release buffer slot 0 but its state was 0
01-01 00:38:47.632 208 252 E FslCameraHAL: getGpsCoordinates: error reading jpeg Coordinates tag
01-01 00:38:47.633 208 252 E FslCameraHAL: getGpsTimeStamp: error reading jpeg TimeStamp tag
01-01 00:38:47.633 208 252 E FslCameraHAL: getGpsProcessingMethod: error reading jpeg ProcessingMethod tag
01-01 00:38:47.633 208 252 E FslCameraHAL: rudolph Max number of EXIF elements already inserted 1
01-01 00:38:47.633 208 252 E FslCameraHAL: rudolph Max number of EXIF elements already inserted 1
01-01 00:38:47.633 208 252 E FslCameraHAL: rudolph Max number of EXIF elements already inserted 1
01-01 00:38:47.633 208 252 E FslCameraHAL: rudolph Max number of EXIF elements already inserted 1
01-01 00:38:47.633 208 252 E FslCameraHAL: rudolph Max number of EXIF elements already inserted 1
01-01 00:38:47.633 208 252 E FslCameraHAL: rudolph Max number of EXIF elements already inserted 1
01-01 00:38:47.633 208 252 E FslCameraHAL: rudolph add for jpegRotation=0
01-01 00:38:47.633 208 252 E FslCameraHAL: rudolph add for degreesToExifOrientation degrees=0
01-01 00:38:47.633 208 252 E FslCameraHAL: rudolph add for exif_orient to insertElement exif_orient=1
01-01 00:38:47.633 208 252 E FslCameraHAL: rudolph Max number of EXIF elements already inserted 1
01-01 00:38:47.635 1332 1926 I CameraDeviceState: Legacy camera service transitioning to state CAPTURING
01-01 00:38:47.636 1332 1926 E CameraDeviceState: Cannot call capture while in state: 0
01-01 00:38:47.645 208 825 E Camera2Client: startPreviewL: Can't start preview in state STILL_CAPTURE
01-01 00:38:47.647 1332 1924 E RequestThread-0: Received device exception during capture call:
01-01 00:38:47.647 1332 1924 E RequestThread-0: java.lang.RuntimeException: startPreview failed
01-01 00:38:47.647 1332 1924 E RequestThread-0: at android.hardware.Camera.startPreview(Native Method)
01-01 00:38:47.647 1332 1924 E RequestThread-0: at android.hardware.camera2.legacy.RequestThreadManager.startPreview(RequestThreadManager.java:288)
01-01 00:38:47.647 1332 1924 E RequestThread-0: at android.hardware.camera2.legacy.RequestThreadManager.doPreviewCapture(RequestThreadManager.java:330)
01-01 00:38:47.647 1332 1924 E RequestThread-0: at android.hardware.camera2.legacy.RequestThreadManager.-wrap3(RequestThreadManager.java)
01-01 00:38:47.647 1332 1924 E RequestThread-0: at android.hardware.camera2.legacy.RequestThreadManager$5.handleMessage(RequestThreadManager.java:802)
01-01 00:38:47.647 1332 1924 E RequestThread-0: at android.os.Handler.dispatchMessage(Handler.java:98)
01-01 00:38:47.647 1332 1924 E RequestThread-0: at android.os.Looper.loop(Looper.java:148)
01-01 00:38:47.647 1332 1924 E RequestThread-0: at android.os.HandlerThread.run(HandlerThread.java:61)
01-01 00:38:47.712 208 431 W audio_hw_primary: out_set_parameters routing=2, ret 0, out -1243028160
01-01 00:38:47.722 208 430 W audio_hw_primary: ret -32, pcm write 768 error wait error: hw 0x25080 app 0x25680 avail 0x0
01-01 00:38:47.722 208 430 W audio_hw_primary: : Unknown error -32
01-01 00:38:47.899 511 521 I art : Background partial concurrent mark sweep GC freed 18349(1333KB) AllocSpace objects, 26(536KB) LOS objects, 33% free, 5MB/8MB, paused 2.076ms total 134.883ms
01-01 00:38:47.906 208 1412 E BufferQueueConsumer: [GraphicBufferSource] releaseBuffer: attempted to release buffer slot 3 but its state was 0
01-01 00:38:47.966 208 1412 E BufferQueueConsumer: [GraphicBufferSource] releaseBuffer: attempted to release buffer slot 2 but its state was 0
01-01 00:38:48.272 511 525 W ActivityManager: Activity pause timeout for ActivityRecord{fd441d u0 com.android.camera2/com.android.camera.CameraLauncher t7 f}
01-01 00:38:48.367 197 509 E BufferQueueProducer: [com.android.launcher/com.android.launcher2.Launcher] dequeueBuffer: can't dequeue multiple buffers without setting the buffer count
01-01 00:38:48.927 1173 1232 W OpenGLRenderer: Incorrectly called buildLayer on View: ShortcutAndWidgetContainer, destroying layer...
01-01 00:38:49.466 208 252 I FslCameraHAL: insertExifThumbnailImage. ReplaceThumbnail(). ret=1
01-01 00:38:49.537 1332 1906 I RequestThread-0: Received jpeg.
01-01 00:38:49.537 1332 1906 W CaptureCollector: jpegProduced called with no jpeg request on queue!
01-01 00:38:49.537 1332 1906 E RequestThread-0: Dropping jpeg frame.
01-01 00:38:50.816 208 431 W audio_hw_primary: no standby

Labels (3)
0 Kudos
Reply
2 Replies

960 Views
joanxie
NXP TechSupport
NXP TechSupport

what framerate and data format do you use? IPU can support up to 240M, which depends what framerate and data format you use.

0 Kudos
Reply

960 Views
rudolphhsueh
Contributor III

Hi Joan,

     From my log message. Framerate is 15 and data format is YUYV. Thanks.

0 Kudos
Reply