Hello,
I have a question about the release notes of imx-yocto-L4.14.98_2.3.1. You have written that the tested version for imx-gpu-g2d is 6.2.4.p4.8. I am unable to request the file because it cannot be found. For example "wget http://www.freescale.com/lgfiles/NMG/MAD/YOCTO/imx-gpu-g2d-6.2.4.p4.8.bin". Do you forget to upload the file or is there a new path to request the file?
regards,
Patrick
If I use
https://www.nxp.com/lgfiles/NMG/MAD/YOCTO//imx-gpu-g2d-6.2.4.p4.8-arm.bin
it works. Can you confirm that this is the 32-bit variant?
I´m wondering for imx-gpu-viv the files called
regards
You don't have to build it, but it will be downloaded automatically if your board has g2d, like imx6q or imx8mm.
Yes of course but that wasn´t exactly my question. The version from the manual "i.MX_Linux_Release_Notes" is imx-gpu-g2d-6.2.4.p4.8.bin. When I try to download manually "wget https://www.nxp.com/lgfiles/NMG/MAD/YOCTO/imx-gpu-g2d-6.2.4.p4.8.bin" then I get the message file not found. So that´s why I ask you if you can confirm that the links below are correct?
aarch32: https://www.nxp.com/lgfiles/NMG/MAD/YOCTO/imx-gpu-g2d-6.2.4.p4.8-arm.bin
aarch64: https://www.nxp.com/lgfiles/NMG/MAD/YOCTO/imx-gpu-g2d-6.2.4.p4.8-aarch64.bin
regards,
Patrick
Hi Patrick,
Yes, you are right, I have confirmed it for you, for aarch32, you now need to append "-arm" instead of "-aarch32".
aarch32:https://www.nxp.com/lgfiles/NMG/MAD/YOCTO//imx-gpu-g2d-6.2.4.p4.8-arm.bin
aarch64: https://www.nxp.com/lgfiles/NMG/MAD/YOCTO/imx-gpu-g2d-6.2.4.p4.8-aarch64.bin
Have nice day
Best Regards
Rita
Thank you very much but what should I use for 32-bit CPUs like i.MX6?
https://www.nxp.com/lgfiles/NMG/MAD/YOCTO//imx-gpu-g2d-6.2.4.p4.8-aarch32.bin
doesn´t work.
regards,
Patrick