imx RT1176 bootable image config

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

imx RT1176 bootable image config

ソリューションへジャンプ
572件の閲覧回数
Kris_chao
Contributor III

您好,新手想请教一下,怎么让程序从NOR FLASH存储器中拷贝进RAM进行非XIP启动,bootable image要怎么配置和生成,MCUXpresso要怎么设置才能编译出来?我看XIP启动,直接能编译出符合格式的bootable image文件,但是非XIP启动不知道怎么操作?

0 件の賞賛
返信
1 解決策
569件の閲覧回数
jeremyzhou
NXP Employee
NXP Employee

Hi,
非常感谢使用NXP产品,很高兴为你提供技术支持!
具体方法请参考此贴
Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
570件の閲覧回数
jeremyzhou
NXP Employee
NXP Employee

Hi,
非常感谢使用NXP产品,很高兴为你提供技术支持!
具体方法请参考此贴
Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信