Hi,
I am using the iMX8MP and I have a codec connected to SAI1 which requires the MCLK to be present before codec is setup. Codec is connected to iMX8MP so that codec uses SAI1_MCLK pin. iMX8MP is the master in the system providing MCLK, BCLK and WCLK.
I have tried various things to make MCLK start before codec is setup via I2C or to make it continuous, but MCLK is not started until capture is started (eg. with arecord). See screenshot below.
I have tried to move clk_prepare_enable(mclk); to probe of codec driver without luck. I think the MCLK might be gated by SAI1 somehow.
Some register dumps when system is idle. Looks like SAI1 is enabled
devmem 0x30c10100 0xC0000000
devmem 0x30e20000 0x04000002
Is there a way to start MCLK before I2C commands? Alternatively, have it run continuously.
BR,
Ulrich
解決済! 解決策の投稿を見る。
Hello @ulrich_sorensen
One can try modifying the fsl_sai.c in fsl_sai_probe function:
clk_prepare_enable(sai->bus_clk);
clk_prepare_enable(sai->mclk_clk[1]);
regmap_update_bits(sai->regmap, FSL_SAI_MCTL,
FSL_SAI_MCTL_MCLK_EN, FSL_SAI_MCTL_MCLK_EN);
regmap_update_bits(sai->regmap, FSL_SAI_TCSR(8),
FSL_SAI_CSR_TERE, FSL_SAI_CSR_TERE);
After of modifiying the sai MCLK should be active when the system bootup.
But after sai driver callback ends (e.g aplay ends), MCLK will be de-active again. The reason is that in sai trigger stop, the transmitter is disabled. To keep the MCLK always on, need to keep transmitter always on.
In a few words, do not clear FSL_SAI_CSR_TERE in trigger stop.
I hope this information can helps to you.
Best regards,
Salas.
Hello @ulrich_sorensen
One can try modifying the fsl_sai.c in fsl_sai_probe function:
clk_prepare_enable(sai->bus_clk);
clk_prepare_enable(sai->mclk_clk[1]);
regmap_update_bits(sai->regmap, FSL_SAI_MCTL,
FSL_SAI_MCTL_MCLK_EN, FSL_SAI_MCTL_MCLK_EN);
regmap_update_bits(sai->regmap, FSL_SAI_TCSR(8),
FSL_SAI_CSR_TERE, FSL_SAI_CSR_TERE);
After of modifiying the sai MCLK should be active when the system bootup.
But after sai driver callback ends (e.g aplay ends), MCLK will be de-active again. The reason is that in sai trigger stop, the transmitter is disabled. To keep the MCLK always on, need to keep transmitter always on.
In a few words, do not clear FSL_SAI_CSR_TERE in trigger stop.
I hope this information can helps to you.
Best regards,
Salas.