iMX8 X Secure Debug Usage Guide

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

iMX8 X Secure Debug Usage Guide

跳至解决方案
992 次查看
wdcrith
Contributor II

Hello NXP,

I am working on a custom piece of hardware which uses the iMX8 X (specifically the IMX8 DX) SOC. I am looking for guidance on how to test out the secure debug (secure JTAG) function of the processor.

I have found references to other application notes aimed at the IMX8M, but no such document for the IMX8 X.

Help in locating the correct document or usage guide would be appreciated.

Thanks

0 项奖励
回复
1 解答
931 次查看
wdcrith
Contributor II

Thanks, good to know that the IMX8X secure debug is similar in function to the IMX8M.

Looking into this more it appears that steps are provided for secure debug usage in the application note AN12631 (section 6)


Normal and Secure Debug for i.MX8/8X Family of Applications Processors

 

Though that application note references Lauterbach debugger scripts for handling the secure debug handshaking. Which sounds like those scripts are only available via direct contact to Lauterbach or by opening a support request with NXP for those script files.

That info was found here: https://community.nxp.com/t5/i-MX-Processors/Lauterbach-scripts-for-i-MX8/m-p/1135278

 

Thanks for the help.

在原帖中查看解决方案

0 项奖励
回复
2 回复数
937 次查看
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello,

There is security reference manual that need nda to access but in general the JTAG is the same as MX8M.

regards

0 项奖励
回复
932 次查看
wdcrith
Contributor II

Thanks, good to know that the IMX8X secure debug is similar in function to the IMX8M.

Looking into this more it appears that steps are provided for secure debug usage in the application note AN12631 (section 6)


Normal and Secure Debug for i.MX8/8X Family of Applications Processors

 

Though that application note references Lauterbach debugger scripts for handling the secure debug handshaking. Which sounds like those scripts are only available via direct contact to Lauterbach or by opening a support request with NXP for those script files.

That info was found here: https://community.nxp.com/t5/i-MX-Processors/Lauterbach-scripts-for-i-MX8/m-p/1135278

 

Thanks for the help.

0 项奖励
回复