Hello NXP,
I am working on a custom piece of hardware which uses the iMX8 X (specifically the IMX8 DX) SOC. I am looking for guidance on how to test out the secure debug (secure JTAG) function of the processor.
I have found references to other application notes aimed at the IMX8M, but no such document for the IMX8 X.
Help in locating the correct document or usage guide would be appreciated.
Thanks
已解决! 转到解答。
Thanks, good to know that the IMX8X secure debug is similar in function to the IMX8M.
Looking into this more it appears that steps are provided for secure debug usage in the application note AN12631 (section 6)
Normal and Secure Debug for i.MX8/8X Family of Applications Processors
Though that application note references Lauterbach debugger scripts for handling the secure debug handshaking. Which sounds like those scripts are only available via direct contact to Lauterbach or by opening a support request with NXP for those script files.
That info was found here: https://community.nxp.com/t5/i-MX-Processors/Lauterbach-scripts-for-i-MX8/m-p/1135278
Thanks for the help.
Thanks, good to know that the IMX8X secure debug is similar in function to the IMX8M.
Looking into this more it appears that steps are provided for secure debug usage in the application note AN12631 (section 6)
Normal and Secure Debug for i.MX8/8X Family of Applications Processors
Though that application note references Lauterbach debugger scripts for handling the secure debug handshaking. Which sounds like those scripts are only available via direct contact to Lauterbach or by opening a support request with NXP for those script files.
That info was found here: https://community.nxp.com/t5/i-MX-Processors/Lauterbach-scripts-for-i-MX8/m-p/1135278
Thanks for the help.