iMX7D + WiFi (Marvell 88W8897) WIFI Direct is functional ?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

iMX7D + WiFi (Marvell 88W8897) WIFI Direct is functional ?

1,158 次查看
jbnadal
Contributor I

Hello,

We are using an imx7D SOC with Wi-Fi Module (Marvell 88W8897).

With:

- a Linux BSP (Linux 4.1.15).

- WiFI mwifiex 1.0 (15.87.19.p14)

WPA Supplicant v2.7 with P2P support.

driver are launch in mode 7
modprobe mwifiex driver_mode=0x7

Is Wi-Fi direct is functional with this chip ?

for me I could found P2P device with p2p_find but I could connect (Failed to create AP).

Is some one has already use it with this couple ?( SOC + WIFI Driver) ?

With supplicant or marvell tool ?


Best Regards

 

标签 (2)
0 项奖励
回复
1 回复

1,141 次查看
IvanRuiz
NXP Employee
NXP Employee

Hello,

 

It seems that iMX7D has support for wifi in L5.4.47. Check those dtses: https://source.codeaurora.org/external/imx/linux-imx/tree/arch/arm/boot/dts/imx7d-sdb-pcie-ep.dts?h=... and https://source.codeaurora.org/external/imx/linux-imx/tree/arch/arm/boot/dts/imx7d-sdb-usd-wifi.dts?h... . Please note that for PCIe full Mini PCie a Wifi card is needed and I am not aware about any Marvell Wifi card with mini PCIe connector.

 

 

Note: L4.1.15 is not supported anymore by Standard Support, so if you decide to continue with this version, paid support can be provided by i.MX Professional Services: https://www.nxp.com/support/support/nxp-engineering-services/professional-engineering-services:PROFE...

 

Hope it helps!

 

BR,

Ivan.

0 项奖励
回复