Dear community,
We have been developing our product with iMX7D.
I am checking a Serial Audio Interface.
I hope to get a SAIx_CLK_ROOT minimum frequency value.
In the the Reference Manual IMX7DRM: Table 5-11. Clock Root Table,
it is described that the SAIx_CLK_ROOT MAX frequency value is 67.5 MHz.
But I could not find the SAIx_CLK_ROOT MIN frequency value .
[Question]
Could you tell me the SAIx_CLK_ROOT minimum frequency value ?
Best Regards,
Koichi Sakagami
Solved! Go to Solution.
Hi Kochi,
In Table 5-11. Clock Root Table you can see all the available clock sources for SAI. The input with lowest frequency is 24MHz (000 - OSC_24M).
Then in Figure 5-15. CCM Clock Tree Root Slices you can find that SAIx_CLK_ROOT has a pre-divider and post-divider.
Finally in chapter 5.2.8.10 Target Register (CCM_TARGET_ROOTn) you can se that pre divider is 3 bits and post divider is 6 bits. So you can divide the 24MHz signal by 8 and then by 64 which is 45kHz approximately.
Regards,
Carlos
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Kochi,
In Table 5-11. Clock Root Table you can see all the available clock sources for SAI. The input with lowest frequency is 24MHz (000 - OSC_24M).
Then in Figure 5-15. CCM Clock Tree Root Slices you can find that SAIx_CLK_ROOT has a pre-divider and post-divider.
Finally in chapter 5.2.8.10 Target Register (CCM_TARGET_ROOTn) you can se that pre divider is 3 bits and post divider is 6 bits. So you can divide the 24MHz signal by 8 and then by 64 which is 45kHz approximately.
Regards,
Carlos
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------