iMX7D : SAIx_CLK_ROOT minimum frequency value for SAI (Serial Audio Interface )module

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

iMX7D : SAIx_CLK_ROOT minimum frequency value for SAI (Serial Audio Interface )module

跳至解决方案
2,306 次查看
koichisakagami
Contributor II

Dear community,
We have been developing our product with iMX7D.

I am checking a Serial Audio Interface.
I hope to get a SAIx_CLK_ROOT minimum frequency value.

In the the Reference Manual IMX7DRM: Table 5-11. Clock Root Table,
it is described that the SAIx_CLK_ROOT MAX frequency value is 67.5 MHz.
But I could not find the  SAIx_CLK_ROOT MIN frequency value .

[Question]
        Could you tell me the SAIx_CLK_ROOT minimum frequency value ?

Best Regards,
       Koichi Sakagami

标签 (1)
0 项奖励
回复
1 解答
1,989 次查看
Carlos_Musich
NXP Employee
NXP Employee

Hi Kochi,

In Table 5-11. Clock Root Table you can see all the available clock sources for SAI. The input with lowest frequency is 24MHz (000 - OSC_24M).

Then in Figure 5-15. CCM Clock Tree Root Slices you can find that SAIx_CLK_ROOT has a pre-divider and post-divider.

pastedImage_1.png

Finally in chapter 5.2.8.10 Target Register (CCM_TARGET_ROOTn) you can se that pre divider is 3 bits and post divider is 6 bits. So you can divide the 24MHz signal by 8 and then by 64 which is 45kHz approximately.


Regards,
Carlos

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,990 次查看
Carlos_Musich
NXP Employee
NXP Employee

Hi Kochi,

In Table 5-11. Clock Root Table you can see all the available clock sources for SAI. The input with lowest frequency is 24MHz (000 - OSC_24M).

Then in Figure 5-15. CCM Clock Tree Root Slices you can find that SAIx_CLK_ROOT has a pre-divider and post-divider.

pastedImage_1.png

Finally in chapter 5.2.8.10 Target Register (CCM_TARGET_ROOTn) you can se that pre divider is 3 bits and post divider is 6 bits. So you can divide the 24MHz signal by 8 and then by 64 which is 45kHz approximately.


Regards,
Carlos

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复