Hi
I am not able to boot to android using the image provided on freescale website for eMMC:
Below are my steps:
1. Copy the following files in release_package/image_*/sabresd_6dq to your MFGTool-Dir/Profiles/MX6Q Linux
Update/OS Firmware/files/android/ directory.
eMMC/boot.img
u-boot-6q.bin and renamed it to u-boot.bin
eMMC/system.bin
eMMC/recovery.bin
2. Change the SABRE SD SW6 (boot) to 00001100 (from 1-8 bit) to enter download mode.
3. And download the images by MFGTool
4. Download sucessful.
5.Change Boot Switch (SW6) to 11010110 (from 1-8 bit) to switch the board back to eMMC boot mode.
6. Reset
7. Tried to set/change environment variables according to the Android_User_Manual.pdf
Please help,
thanks.
Attached is the log messages
Original Attachment has been moved to: putty.log.zip
解決済! 解決策の投稿を見る。
The first line of your log has weird characters but I was able to read it with vim. the eMMC image should work out of the box. Just to make sure, what are the u-boot commands you executed? There is a newer version of JB422_110, try it also.
Leo
Dear floriang,
I have same problem,
Are you into Android shell now?
How do you slove this probem?
Is modify "u-boot commands" ?
I check JB422_110 FAQ , and fill the u-boot commands :
setenv bootargs console=ttymxc0,115200 init=/init video=mxcfb0
video=mxcfb1:off video=mxcfb2:off fbmem=10M fb0base=0x17b00000
gpumem=96M vmalloc=400M androidboot.console=ttymxc0
but the problem is exist.
What are you change?
Could you kindly tell me?
Thanks a lot.
Hello Jeffrey,
Depending on the board the image may not work. I was successful using Sabre "Platform (the ones with the LCD attached), but I have only one Sabre Board, working correctly with Jellybean image
http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=RDIMX6SABREBRD&fpsp=1&tab=Design_Tool...
(android_jb4.2.2_1.1.0-ga_image_bundle.tar.gz)
I suggest you try the android images of the link above with a Sabre "Platform" if you didn't try yet, and try starting another thread if you still have troubles.
Dear Floriang,
Thanks your quick respond.
I am devlopment on our board similar with SABRE board.
I base on the android_jb4.2.2_1.1.0-ga_image_bundle.tar.gz to devlopment.
But our board only 512MB.
so I set my u-boot command line as below:
MX6SDL SABRESD U-Boot > printenv
bootdelay=3
baudrate=115200
ipaddr=192.168.1.103
serverip=192.168.1.101
netmask=255.255.255.0
loadaddr=0x10800000
rd_loadaddr=0x11000000
netdev=eth0
ethprime=FEC0
splashimage=0x30000000
splashpos=m,m
lvds_num=1
ethact=FEC0
bootargs=console=ttymxc0,115200 init=/init video=mxcfb0:dev=ldb,bpp=32 video=mxcfb1:off video=mxcfb2:off fbmem=10M fb0base=0x17b00000 gpumem=96M vmalloc=400M androidboot.console=ttymxc0 androidboot.hardware=freescale ldb=sin0
stdin=serial
stdout=serial
stderr=serial
fastboot_dev=mmc2
bootcmd=booti mmc2
You seem OK on JB422_110, but I am failure.
Do you use same u-boot command line?
(PS: our display is output to LVDS0, so I set ldb=sin0)
Below is stop debug message of my image:
ehci_fsl_bus_suspend begins, Host 1
ehci_fsl_bus_suspend ends, Host 1
warning: `zygote' uses 32-bit capabilities (legacy support in use)
request_suspend_state: wakeup (3->0) at 20502714005 (1970-01-02 00:00:08.690542668 UTC)
eth0: no PHY, assuming direct connection to switch
PHY 0:00 not found
eth0: could not attach to PHY
acc_open
acc_release <
Hi!
I was not able to get anything working with ICS, so I gave a try to jellybean.
Jellybean woks fine, and I was able to compile an engineering build of android and write to the eMMC by following the user guide.
I think ICS is broken.
The first line of your log has weird characters but I was able to read it with vim. the eMMC image should work out of the box. Just to make sure, what are the u-boot commands you executed? There is a newer version of JB422_110, try it also.
Leo
Edit2:
Using exactly the same steps and the jellybean images (4.2.2) from freescale, I can write successfully to eMMC or SD card, and everything seems to work fine.
Is the ICS image from freescale broken?
I will try to compile my own image to see if it changes anything...
Edit:
I am using the r13.4.1 image (with ICS).
Also I tried to write to the SD card with the manufacturing tools without success.
From the sd card, I am able to boot to the OS sometimes, but the OS freezes after 1-2minute.
When the OS freeze, I get the kind of messages below:
binder: release 2506:2506 transaction 20667 out, still active
binder: 2387:2667 transaction failed 29189, size 584-8
binder: 2988:2999 transaction failed 29189, size 292-0
binder: release 2988:2988 transaction 21177 out, still active
request_suspend_state: sleep (0->3) at 163926767689 (1970-01-02 00:02:16.179447349 UTC)
stop_drawing_early_suspend: timeout waiting for userspace to stop drawing
binder: release 2387:2665 transaction 21178 out, still active
binder: release 2387:2665 transaction 21177 in, still active
binder: release 2387:2666 transaction 21224 in, still active
binder: send failed reply for transaction 21224 to 2837:2858
binder: release 2387:3009 transaction 21208 in, still active
binder: send failed reply for transaction 21208 to 3011:3011
binder: 2837:2858 transaction failed 29189, size 532-0
alarm_release: clear alarm, pending 0
alarm_release: clear alarm, pending 0
alarm_release: clear alarm, pending 0
request_suspend_state: wakeup (3->0) at 171893651356 (1970-01-02 00:02:24.146329683 UTC)
binder: release 2272:2272 transaction 20667 in, still active
binder: send failed reply for transaction 20667, target dead
binder: release 2272:2372 transaction 21178 in, still active
init: untracked pid 2269 exited
init: untracked pid 2272 exited
....
init: untracked pid 2596 exited
request_suspend_state: wakeup (0->0) at 178214894357 (1970-01-02 00:02:30.467573685 UTC)
acc_open
acc_release