iMX6Q: HDMI not working

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

iMX6Q: HDMI not working

5,733 次查看
pj0585
Contributor III

Hello,

I'm working on a custom iMX6Q board (similar to imx6 sabre smart device). HDMI is not working when display connected using DVI-D connector. I'm using LTIB based linux image (linux 3.0.35)

- HDMI hot plug feature is working (verfied through /sys/class/devices/....)

- EDID information is read out correctly

- HDMI_CEC feature is disabled

- I have observed the HDMI_PHY_STAT0 register. The RX_SENSE bits remain low. Could not figure out what that indicates as iMX6 datasheet does not give much information.

- HDMI data & clock lines remain low when probed using oscilloscope.

Any inputs will be of help to me.

-Pj

标签 (2)
标记 (1)
0 项奖励
回复
9 回复数

1,908 次查看
varsmolta
Contributor V
0 项奖励
回复

1,908 次查看
kelvinchan
Contributor I

Hi Prasant,

     Do you solve this issue now?

     I got the same problem as this issue

     Could you share the information about this?

Many thanks,

Kelvin

0 项奖励
回复

1,908 次查看
pj0585
Contributor III

Hi Kelvin,

Sorry for late reply, I saw this thread only today.

Case your issue is not yet solved:

Mine was a hardware design issue (nothing in software) and it is fixed now. Which ESD Protection chip are you using?

-Pj

0 项奖励
回复

1,908 次查看
ramakrishnanven
Contributor II

I am facing the same issue for the past one week. I have used a HDMI to VGA converter and connected a VGA display. I could not see any thing in my VGA monitor. Can you help me about what and how to configure the display

0 项奖励
回复

1,908 次查看
dlschaeffer
Contributor II

I'm having a similar issue with a TI TDP12S521 ESD protection chip

0 项奖励
回复

1,908 次查看
pj0585
Contributor III

@Daniel,

Is yout HDMI Hot plug detect working?

-Pj

0 项奖励
回复

1,908 次查看
dlschaeffer
Contributor II

It was a hardware issue. Hot Plug was working but the ESD chip wasn't wired up correctly. I'm using a differnt ESD chip but this thread details the same issue No display on HDMI Panel

0 项奖励
回复

1,908 次查看
Yuri
NXP Employee
NXP Employee

Please use "true" HDMI connection (not HDMI-DVI adapter)

0 项奖励
回复

1,908 次查看
SandorYu
NXP Employee
NXP Employee

Please check the IPU DI clock whether is enable firstly.

The HDMI PHY work depend on pixel clock.

0 项奖励
回复