Hello,
I'm working on a custom iMX6Q board (similar to imx6 sabre smart device). HDMI is not working when display connected using DVI-D connector. I'm using LTIB based linux image (linux 3.0.35)
- HDMI hot plug feature is working (verfied through /sys/class/devices/....)
- EDID information is read out correctly
- HDMI_CEC feature is disabled
- I have observed the HDMI_PHY_STAT0 register. The RX_SENSE bits remain low. Could not figure out what that indicates as iMX6 datasheet does not give much information.
- HDMI data & clock lines remain low when probed using oscilloscope.
Any inputs will be of help to me.
-Pj
Hi Prasant,
Do you solve this issue now?
I got the same problem as this issue
Could you share the information about this?
Many thanks,
Kelvin
Hi Kelvin,
Sorry for late reply, I saw this thread only today.
Case your issue is not yet solved:
Mine was a hardware design issue (nothing in software) and it is fixed now. Which ESD Protection chip are you using?
-Pj
I am facing the same issue for the past one week. I have used a HDMI to VGA converter and connected a VGA display. I could not see any thing in my VGA monitor. Can you help me about what and how to configure the display
I'm having a similar issue with a TI TDP12S521 ESD protection chip
It was a hardware issue. Hot Plug was working but the ESD chip wasn't wired up correctly. I'm using a differnt ESD chip but this thread details the same issue No display on HDMI Panel