Customer is designing the mx25 in a system that utilizes a ‘smart’ battery charger. He routes D+/D- from the input port of the device to both the charger and MX25. The charger listens to D+/D- and complies to the BC1.2 spec.
The system will operate in a few different modes where the mx25 may or may not be powered (the charger has dynamic power path management to route HOST power to our system or directly to the battery or both.).
As I understand the charger, at initial plugin it will apply 600mV bias voltages to determine the state of the D+/D- lines to determine current limits.
Does 600mV on USBPHY1_DP/USBPHY1_DM matter to an unpowered MX25?
Gordy
解決済! 解決策の投稿を見る。
Hi Gordon
it is not allowed to apply to unpowered i.MX25 any
voltages (may damage chip or cause malfunction).
Only in i.MX6 VBUS can be applied to unpowered processor,
IMX6DQCEC p.31
Best regards
igor
Hi Gordon
it is not allowed to apply to unpowered i.MX25 any
voltages (may damage chip or cause malfunction).
Only in i.MX6 VBUS can be applied to unpowered processor,
IMX6DQCEC p.31
Best regards
igor
Thank You!