iMX25 USB PHY Dm Dp voltage levels (unpowered)

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

iMX25 USB PHY Dm Dp voltage levels (unpowered)

Jump to solution
1,175 Views
GordyCarlson
NXP Employee
NXP Employee

 

Customer is designing the mx25 in a system that utilizes a ‘smart’ battery charger.  He routes D+/D- from the input port of the device to both the charger and MX25.  The charger listens to D+/D- and complies to the BC1.2 spec.

The system will operate in a few different modes where the mx25 may or may not be powered (the charger has dynamic power path management to route HOST power to our system or directly to the battery or both.).

As I understand the charger, at initial plugin it will apply 600mV bias voltages to determine the state of the D+/D- lines to determine current limits.


Does 600mV on USBPHY1_DP/USBPHY1_DM matter to an unpowered MX25?

    1. Does the answer depend on whether state of USBPHY1_VBUS?
      1. USBPHY1_VBUS = 0V OR
      2. USBPHY1_VBUS = 5V from usb bus….. rest of MX25 would remain at 0V.

Gordy

Labels (1)
0 Kudos
Reply
1 Solution
773 Views
igorpadykov
NXP Employee
NXP Employee

Hi Gordon

it is not allowed to apply to unpowered i.MX25 any

voltages (may damage chip or cause malfunction).

Only in i.MX6 VBUS can be applied to unpowered processor,

IMX6DQCEC p.31

Best regards

igor

View solution in original post

0 Kudos
Reply
2 Replies
774 Views
igorpadykov
NXP Employee
NXP Employee

Hi Gordon

it is not allowed to apply to unpowered i.MX25 any

voltages (may damage chip or cause malfunction).

Only in i.MX6 VBUS can be applied to unpowered processor,

IMX6DQCEC p.31

Best regards

igor

0 Kudos
Reply
773 Views
GordyCarlson
NXP Employee
NXP Employee

Thank You!

0 Kudos
Reply