Hi:
I intend to use the CAN bus of i.mx8m plus with Windows 10 IoT.
But it doesn't work at all.
1. I connected the CAN1 and CAN2 to check it and execute the a and b roles with example "FlexCAN-interrupt-source" (from NXP's SW package),
there's any response at the role-b.
2. Disconnect the CAN1 from CAN2, observe the signal with a logic analyser, nothing happened one the role-a sent.
For this, I add debug info and re-build the project "imxcan_mc", the flow seems good,
ImxCanIoctlControllerSendNonBlocking=>FLEXCAN_TransferSendNonBlocking=>FLEXCAN_WriteTxMb
But I cannot get any signal on the CANBUS.
I also test the hardware with Yocto project,
It works fine in the above 2 condition.
Can somebody help?
已解决! 转到解答。
Hi:
I'm really sorry for my mistake for this post,
It's about the H/W connection,
There is a switch between the i.mx8 and the terminal connector,
The switch should be enabled to establish the connection.
Thank you all..
@ChrisChang1234 hello,
that is great news!
I was about to suggest some ideas but you have been a bit quicker.
Can you please let us know what was the problem?
With regards
Ludek
Hi:
I'm really sorry for my mistake for this post,
It's about the H/W connection,
There is a switch between the i.mx8 and the terminal connector,
The switch should be enabled to establish the connection.
Thank you all..
Hi @ChrisChang1234 ,
I hope you're doing well!
Unfortunately, Windows 10 IoT Enterprise isn't currently supported for custom boards, only EVKs. I apologize for the inconvenience this may cause. Thank you.
Best regards,
Hector.
Hi @ChrisChang1234 .
I hope you're doing well! I've contacted or W10 IoT team for any input on this issue.
In the meantime, could you please let me know if you're using a custom board or an EVK?
Best regards,
Hector.