*****@*****:~/Projects/yocto$ repo init -u https://github.com/nxp-imx/imx-manifest -b imx-linux-rocko -m imx-4.9.88-2.0.0_ga.xml
Your identity is: *** *** <***@***>
If you want to change this, please re-run 'repo init' with --config-name
Testing colorized output (for 'repo diff', 'repo status'):
black red green yellow blue magenta cyan white
bold dim ul reverse
Enable color display in this user account (y/N)? y
repo has been initialized in /home/*****/Projects/yocto
*****@*****:~/Projects/yocto$ repo sync
remote: Enumerating objects: 1469, done.
remote: Counting objects: 0% (1/594)
remote: Counting objects: 1% (6/594)
remote: Counting objects: 2% (12/594)
remote: Counting objects: 3% (18/594)
...
..
.
Resolving deltas: 98% (989/1009)
Resolving deltas: 99% (999/1009)
Resolving deltas: 100% (1009/1009)
Resolving deltas: 100% (1009/1009), completed with 67 local objects.
Fetching: 0% (0/9) 0:51 | 2 jobs | 0:40 meta-freescale @ sources/meta-freescale
fatal: Couldn't find remote ref refs/tags/rocko-4.9.88-2.0.0_ga_gh
meta-fsl-bsp-release:
fatal: Couldn't find remote ref refs/tags/rocko-4.9.88-2.0.0_ga_gh
meta-fsl-bsp-release: sleeping 4.0 seconds before retrying
fatal: Couldn't find remote ref refs/tags/rocko-4.9.88-2.0.0_ga_gh
error: Cannot fetch meta-fsl-bsp-release from https://github.com/nxp-imx/meta-fsl-bsp-release
Fetching: 100% (9/9), done in 7m51.023s
Fetching: 0% (0/1) 0:05 | 1 job | 0:05 meta-fsl-bsp-release @ sources/meta-fsl-bsp-release
fatal: Couldn't find remote ref refs/tags/rocko-4.9.88-2.0.0_ga_gh
meta-fsl-bsp-release:
fatal: Couldn't find remote ref refs/tags/rocko-4.9.88-2.0.0_ga_gh
meta-fsl-bsp-release: sleeping 4.0 seconds before retrying
fatal: Couldn't find remote ref refs/tags/rocko-4.9.88-2.0.0_ga_gh
error: Cannot fetch meta-fsl-bsp-release from https://github.com/nxp-imx/meta-fsl-bsp-release
Fetching: 100% (1/1), done in 5.764s
error: Cannot checkout meta-fsl-bsp-release: ManifestInvalidRevisionError: revision refs/tags/rocko-4.9.88-2.0.0_ga_gh in meta-fsl-bsp-release not found
error: in `sync`: revision refs/tags/rocko-4.9.88-2.0.0_ga_gh in meta-fsl-bsp-release not found
*****@*****:~/Projects/yocto$
P.S.
Solved! Go to Solution.
Use below revision which is rocko-4.9.88-2.0.0_ga branch , there is no tag about rocko-4.9.88-2.0.0_ga_gh.
<project remote="nxp-imx" revision="75abf98a264aeacf52bdc423dea4886d498ef5ec" name="meta-fsl-bsp-release" path="sources/meta-fsl-bsp-release" >
<linkfile src="imx/tools/fsl-setup-release.sh" dest="fsl-setup-release.sh"/>
<linkfile src="imx/README" dest="README-IMXBSP"/>
</project>
The old BSP manifests are migrated from old server(not github), so these files may need update.
You can try to use rocko-4.9.88-2.0.0_ga branch
Thanks for the quick reply, but I think an error still persists.
You mentioned using the rocko-4.9.88-2.0.0_ga branch, are you sure you mean the imx-linux-rocko branch?
(I'm not familiar with the repo command and am checking to see if I'm right. Sorry if I'm wrong.)
I ran it in the imx-linux-rocko branch with the manifest file imx-4.9.88-2.0.0_ga.xml.
The command itself is executed according to the example at the following URL
https://github.com/nxp-imx/imx-manifest/blob/4fb9b37ff3798243d2690dc7e2f377ae4b6b7dd0/README#L39
And I got an error when I tried to repo sync command.
The error message is
fatal: Couldn't find remote ref refs/tags/rocko-4.9.88-2.0.0_ga_gh
error: Cannot checkout meta-fsl-bsp-release: ManifestInvalidRevisionError: revision refs/tags/rocko-4.9.88-2.0.0_ga_gh in meta-fsl-bsp- release not found
and it seems that rocko-4.9.88-2.0.0_ga_gh is missing.
Note end "_gh" on which manifest requires.
If I am using the wrong branch, we would appreciate it if you could tell us the correc tbranch.
If rocko-4.9.88-2.0.0_ga_gh needs to be updated to run, could you please check and update it?
Thank you in advance.
Use below revision which is rocko-4.9.88-2.0.0_ga branch , there is no tag about rocko-4.9.88-2.0.0_ga_gh.
<project remote="nxp-imx" revision="75abf98a264aeacf52bdc423dea4886d498ef5ec" name="meta-fsl-bsp-release" path="sources/meta-fsl-bsp-release" >
<linkfile src="imx/tools/fsl-setup-release.sh" dest="fsl-setup-release.sh"/>
<linkfile src="imx/README" dest="README-IMXBSP"/>
</project>
The old BSP manifests are migrated from old server(not github), so these files may need update.