Hello, looking for the correct dcd info for i.mx6d pop package w/ lpddr2.
mx6: MCIMX6D5EZK08AE
Memory: EDB8164B4PT-1DAT-F-D
I found the dcd generation script for what I think is correct here:
We're not getting U-boot to proceed past memory initialization though. I suspect there are settings that aren't correct.
Here is what I input into the script:
Manufacturer: | Micron |
Memory part number: | EDB8164B4PT-1DAT-F-D |
Memory type: | LPDDR2-1066 |
DRAM single die density (Gb) | 4 |
DRAM density per Channel (Gb) | 2 |
DRAM Bus Width | 2x32 |
Number of Chip Selects used per Channel | 2 |
DRAM density per CS (Gb) | 1 |
DRAM Bus Width Per Channel | 32 |
Number of Banks | 8 |
Number of ROW Addresses | 14 |
Number of COLUMN Addresses | 10 |
System Information | |
i.Mx Part | i.Mx6D |
MMDC channels: | MMDC0 & MMDC1 |
Bus Width | 64 |
DRAM Clock Freq (MHz) | 400 |
DRAM Clock Cycle Time (ns) | 2.5 |
4KB Interleaving Mode | Interleave |
SI Configuration | |
DRAM DSE Setting - DQ/DQM (ohm) | 240 |
DRAM DSE Setting - ADDR/CMD/CTL (ohm) | 240 |
DRAM DSE Setting - CK (ohm) | 240 |
DRAM DSE Setting - DQS (ohm) | 240 |
Our boot config via GPIO has modified:
boot_cfg3[2] = 1 (ARM 396 mhz)
boot_cfg3[5:4] = 10 (4k interleaving enabled)
I've seen various hints of LPDDR2 memory on imx6 not working in some configurations but can't seem to find a source to figure out if any of those situations apply to our board and whether or not I need to change something. Any suggestions much appreciated.
已解决! 转到解答。
Thank you Igor,
Yes, we figured the part is compatible. We were able to get the part to boot by changing the dcd parameters to be generated from an updated script aid:
https://community.nxp.com/docs/DOC-105965
I found version 1.3 after we had originally found version 0.6. I'm looking for a source article that links to the latest script aid because when searching, for me, the page that linked to the 0.6 version came up as the authoritative version first. After additional searching we found the newer version. I didn't do a diff on the generated dcd information but we are happy that it worked to boot.
We still have an issue that the reported memory by U-boot and to Linux is only 512M even though this part should be reporting 1G of memory. v1.3 page, there is a comment about having the CS0_END parameter calculated incorrectly but I didn't find an updated script. Is 1.3 the latest? If so, I'll dig more into the register itself and see if I can't input the correct value or update the spreadsheet to calculate it correctly.
Hi Dennis
in general EDB8164B4PT should be supported by nxp scm uboot/linux releases
mx6dqscm\freescale\board - uboot-imx - i.MX U-Boot
SCM with suffix "1G0AA" use EDB8164B4PT-1DAT-F-D: MSCMMX6QZDK08AB1G0AA
previous was "1G0A" with MT42L128M64D2LL-25
https://www.mouser.com/datasheet/2/302/SCMIMX6DQCEC-1152074.pdf
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Thank you Igor,
Yes, we figured the part is compatible. We were able to get the part to boot by changing the dcd parameters to be generated from an updated script aid:
https://community.nxp.com/docs/DOC-105965
I found version 1.3 after we had originally found version 0.6. I'm looking for a source article that links to the latest script aid because when searching, for me, the page that linked to the 0.6 version came up as the authoritative version first. After additional searching we found the newer version. I didn't do a diff on the generated dcd information but we are happy that it worked to boot.
We still have an issue that the reported memory by U-boot and to Linux is only 512M even though this part should be reporting 1G of memory. v1.3 page, there is a comment about having the CS0_END parameter calculated incorrectly but I didn't find an updated script. Is 1.3 the latest? If so, I'll dig more into the register itself and see if I can't input the correct value or update the spreadsheet to calculate it correctly.