i.mx53 WinEC7: Switch audio between SGTL5000 and SPDIF

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.mx53 WinEC7: Switch audio between SGTL5000 and SPDIF

774件の閲覧回数
oobin
Contributor I

Dear Experts

I am working @ i.mx53 serires project, OS is windows embedded compact 7 (winec7).


There are two audio output can be utilized in i.mx53 platform.
One is AUDIO_SGTL5000, the other one is SPDIF(through HDMI).
When playing audio, The audio output always comes form AUDIO_SGTL5000.
I must remove AUDIO_SGTL5000 driver to enable SPDIF out.

Some questions:

1) Can I change audio selection from AUDIO_SGTL5000 to SPDIF when playing audio if both driver exist ?

2) Can AUDIO_SGTL5000 and SPDIF both output audio at the same time ?

ラベル(1)
タグ(2)
0 件の賞賛
返信
0 返答(返信)